Skip to main content
markpow
Senior
Jan 17, 2026 4:36 PM UTC
Question

ST-LINK2 on Windows 11

I have worked with ST-LINK/2 on Windows 10 for several years. I must upgrade to Windows 11 because Windows 10 support ended a few months ago. Today, I tried to program the WIO E5 Mini microcontroller, but I found it's impossible because there's no driver for it on my computer.
I found some information that I should install version 9 of that driver. I downloaded it from the original STM source and ran it, but nothing changed. Is till don't see this driver among my devices. Installation ended without any error. 

Is there anybody who can point out what I am missing?

20 replies

MM..1
Super User
Jan 17, 2026 4:51 PM UTC

You mix apples with ... WIO require external STLINK connected to SWD ...

Onboard USB is UART bridge nothink todo with STLINK... Require driver for CP uart bridge.

Specify what is your connection problem.?

markpow
markpowAuthor
Senior
Jan 17, 2026 5:00 PM UTC

I can't upgrade the firmware because of it:

markpow_1-1768669211802.png

There is no item on the list

markpow
markpowAuthor
Senior
Jan 17, 2026 4:58 PM UTC

markpow_0-1768669045813.png

I attached my microcontroller to USB as usual (under W10). As you can see, I use SWD. But the programmer doesn't see it.

 

AScha.3
Super User
Jan 17, 2026 5:53 PM UTC

>who can point out what I am missing?

A working st-link.

Has nothing to do with the CP2102 , uart bridge.

Show a pic of your st-link V2 , then we know what you have.

If you feel a post has answered your question, please click on " Best Answer ".
markpow
markpowAuthor
Senior
Jan 17, 2026 6:11 PM UTC

markpow_0-1768673352162.png

It's the same configuration that has worked under W10. The only change was from W10 to W11.

As you can see, there is no target voltage, and the LED doesn't blink when attached to the USB.

AScha.3
Super User
Jan 17, 2026 6:20 PM UTC

As YOU can see on the CubeProgrammer :

AScha3_0-1768673989590.png

NO st-link connected.

So: you have a st-link at all ? connect it to USB.

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
Jan 17, 2026 6:15 PM UTC

As @AScha.3 said, please show a photo of your ST-Link - you seem to be confusing it with a USB-to-UART adaptor.

 

To start with, check that you have a genuine ST-Link:

How to recognize a genuine ST-LINK/V2 versus a cloned one

 

Then see:

How to solve debugger connection issues

And:

How to solve connection errors when connecting and programming the STM32 target board.

 

A genuine ST-Link should work fine on Windows 11.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Jan 17, 2026 6:29 PM UTC

Here are the possibilities:

If nothing happens in device manager when the device is connected, likely the cable is bad.

"If you feel a post has answered your question, please click ""Accept as Solution""."
markpow
markpowAuthor
Senior
Jan 17, 2026 7:29 PM UTC

I have used the last working pin connections between ST-LINK/2 device and the WIO device, and for now, I'm a little bit closer, I think.
I had such messages earlier, and I recall that there is some kind of magic how to mange it:


20:17:58 : ST-LINK SN : 50FF6B067182575134150187
20:17:58 : ST-LINK FW : V2J45S7
20:17:58 : Board : --
20:17:58 : Voltage : 0.00V
20:17:58 : Error: Unable to get core ID
20:17:58 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

I don't understand how there can be such a small voltage measured by the ST-LINK/2 device. I checked the connections between devices twice, and everything looks fine.

 

AScha.3
Super User
Jan 17, 2026 7:34 PM UTC

>Voltage : 0.00V

means -> you have no power (3v3) at the target, your wio...

connect the 3v3 to wio VDD.

If you feel a post has answered your question, please click on " Best Answer ".