Skip to main content
KiptonM
Senior III
July 18, 2022
Solved

Did ST break SysTick in the last update? It used to work. Now it crashes because I think the interrupt vector is not set. Is this one of those known errors? How do I fix it?

When the SysTick interrupt fires the debugger quits.

I cannot figure out where the NVIC_SetVector statement is for the SysTick. I think it is not set. But I can not find the vector table in the debugger to know for sure.

This used to work, But when I updated to the 1.10.1 IDE and 6.6.1-RC2 Build.20220706-1420. It crashes when the systick interrupt happens.

I am using the STM32G051K8T

This topic has been closed for replies.
Piranha
PiranhaBest answer
Principal III
July 19, 2022

That CubeProgrammer description of nBOOT0 and nBOOT1 options is a nonsense. Again a blind trust without checking the real thing - reference manual...

Look at the RM0444 Rev 5, 2.5 Boot configuration, Table 8. Boot modes.

@Houda GHABRI​ 

30 replies

KnarfB
Super User
July 18, 2022

SysTick is part of the ARM core and its interrupt is enabled in SysTick_Config, see SYST_CSR register. The handler is implicitly set already in the g_pfnVectors table, see startup code and implemented in stm32g0xx_it.c. Works here on a Nucleo G071 board without issues with your tool versions.

hth

KnarfB

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

I tried to look at it in the debugger. it says g_pfnVectors <data variable, no debug info>

KnarfB
Super User
July 18, 2022

You can see the source code in the startup file, startup_stm32g071rbtx.s in my case. The startup file also has a default "do nothing" implementation of SysTick_Handler in the startup file. This "weak" declaration is overridden by SysTick_Handler in stm32g0xx_it.c.

You may check that g_pfnVectors table holds the correct handler address at the SysTick offset by inspecting memory in the debugger.

Don't think that a missing SysTick_Handler is issue.

> the debugger quits

Any output, logs? What if you step at assembly level? A fault?

hth

KnarfB

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

Where should I look for output logs?

It is taking a long time to step until the interrupt fires. I am still working on it. Somewhere around 155 loop iterations. No message, The debugger just stops responding I single step. .

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

I found it in the startup_stm32g051k8tx.s and the vector table looks good.

But when I put a breakpoint in the SysTick_Handler program, the debugger crashes before I get to the interrupt there. It appears the interrupt is going somewhere weird, and crashing. I believe that is the only interrupt active and it is initialized by HAL_Init() and the system crashes shortly after HAL_Init() is executed and I am looping on __NOP(); commands. That is all that is running.

Something is wrong.

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

Here is my code:

int main(void)
{
 /* USER CODE BEGIN 1 */
/*
	{
		uint16_t i, j;
		for (i=0;i<525;i++)
		{
			for (j=0;j<60000;j++) __NOP();
		}
 
	}
*/
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 //SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
// MX_GPIO_Init();
 // MX_DMA_Init();
// MX_ADC1_Init();
// MX_I2C1_Init();
// MX_TIM2_Init();
// MX_TIM3_Init();
// MX_TIM14_Init();
// MX_USART1_UART_Init();
// MX_USART2_UART_Init();
 
 /* Initialize interrupts */
// MX_NVIC_Init();
 /* USER CODE BEGIN 2 */
 
 //__disable_irq();
 /*
 ENCODER_POWER_OFF; // Make sure encoder is off so it can start correctly.
 print_debug_str("Encoder Power Off\r\n");
 
 
 
 TASK_PIN_L;
 TP2_L;
 DIO2_L;
 DIO3_L;
 DIO4_L;
 
 if (isDebug(DEBUG_verify_memory_structures))
 {
	 verify_memory_structures();
 }
*/
 __NOP();
 {
 
	 uint16_t i;
	 for (i=0;i<1000;i++)
	 {
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 20
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 40
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 60
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 80
		 __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); // 100
	 }
 }
 //ADC_init();
 __NOP();

I also put a breakpoint in SysTic_Handler() found in stm32g0xx_it.c but the debugger crashes before I get there.

/**
 * @brief This function handles System tick timer.
 */
void SysTick_Handler(void)
{
 /* USER CODE BEGIN SysTick_IRQn 0 */
 
 /* USER CODE END SysTick_IRQn 0 */
 HAL_IncTick();
 /* USER CODE BEGIN SysTick_IRQn 1 */
 
 /* USER CODE END SysTick_IRQn 1 */
}

Piranha
Principal III
July 18, 2022

Open the memory view at 0x0800003C and check whether it contains the SysTick_Handler() address.

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

0693W00000QLSZtQAP.pngFrom the .map file.

 .text.SysTick_Handler

        0x0000000008005778    0x8 ./Core/Src/stm32g0xx_it.o

        0x0000000008005778        SysTick_Handler

Why is it off by 1? 0x08005779? Should be a number divisible by 4 I would think.

It looks like all the vectors are odd numbers.

The Startup file has:

.section .isr_vector,"a",%progbits
 .type g_pfnVectors, %object
 .size g_pfnVectors, .-g_pfnVectors
 
g_pfnVectors:
 .word _estack
 .word Reset_Handler
 .word NMI_Handler
 .word HardFault_Handler
 .word 0
 .word 0
 .word 0
 .word 0
 .word 0
 .word 0
 .word 0
 .word SVC_Handler
 .word 0
 .word 0
 .word PendSV_Handler
 .word SysTick_Handler
 .word WWDG_IRQHandler /* Window WatchDog */
 .word PVD_IRQHandler /* PVD through EXTI Line detect */
 .word RTC_TAMP_IRQHandler /* RTC through the EXTI line */
 .word FLASH_IRQHandler /* FLASH */
 .word RCC_IRQHandler /* RCC */
 .word EXTI0_1_IRQHandler /* EXTI Line 0 and 1 */
 .word EXTI2_3_IRQHandler /* EXTI Line 2 and 3 */
 .word EXTI4_15_IRQHandler /* EXTI Line 4 to 15 */
 .word 0 /* reserved */
 .word DMA1_Channel1_IRQHandler /* DMA1 Channel 1 */
 .word DMA1_Channel2_3_IRQHandler /* DMA1 Channel 2 and Channel 3 */
 .word DMA1_Ch4_7_DMAMUX1_OVR_IRQHandler /* DMA1 Channel 4 to Channel 7, DMAMUX1 overrun */
 .word ADC1_COMP_IRQHandler /* ADC1, COMP1 and COMP2 */
 .word TIM1_BRK_UP_TRG_COM_IRQHandler /* TIM1 Break, Update, Trigger and Commutation */
 .word TIM1_CC_IRQHandler /* TIM1 Capture Compare */
 .word TIM2_IRQHandler /* TIM2 */
 .word TIM3_IRQHandler /* TIM3 */
 .word TIM6_DAC_LPTIM1_IRQHandler /* TIM6, DAC & LPTIM1 */
 .word TIM7_LPTIM2_IRQHandler /* TIM7 & LPTIM2 */
 .word TIM14_IRQHandler /* TIM14 */
 .word TIM15_IRQHandler /* TIM15 */
 .word TIM16_IRQHandler /* TIM16 */
 .word TIM17_IRQHandler /* TIM17 */
 .word I2C1_IRQHandler /* I2C1 */
 .word I2C2_IRQHandler /* I2C2 */
 .word SPI1_IRQHandler /* SPI1 */
 .word SPI2_IRQHandler /* SPI2 */
 .word USART1_IRQHandler /* USART1 */
 .word USART2_IRQHandler /* USART2 */
 .word LPUART1_IRQHandler /* LPUART1 */

Which looks right.

KnarfB
Super User
July 18, 2022

> Why is it off by 1? 0x08005779? Should be a number divisible by 4 I would think.

LSB 1 indicates thumb mode, looks correct.

KnarfB
Super User
July 18, 2022

You say the debugger crashes. Do you get any useful message from it?

In the Debug Config Debugger tab you can set the ST-LINK freq. Try setting to a low value to compensate for possibly weak ST-LINK connection. There is also a Misc/Log to file checkbox which you might check.

hth

KnarfB

KiptonM
KiptonMAuthor
Senior III
July 18, 2022

So I still do not know why when it calls this interrupt the debugger crashes. I was guessing the vector was wrong, but it appears correct.

I have a breakpoint for the first instruction in the ISR. It never breaks. The debugger just stops about 1 ms after we initialize the SysTick. That is what made me think it was a vector error. But everything looks good.

So I am back to not having a clue as to why it is no longer working. It has been working for more than 6 months, After I upgraded to the new version of IDE and MX it stopped working.