Dear @STTwo-32 , thank you for prompt reply. i have sorted out the issue with my STM32C011F6U6TR (UFQFPN-20) .
It is my soldering temperature of 370 degree (using Hot Air Blower) is too high, and such temperature damages the STM32C011 microcontroller. I replace the dead chip and solder a new one by using 320 degree (Hot air), STM32C011 responds to my STlink-V2.
Ps: I am using STlinkV2 (clone one, 2x5 pins), and also genuine one (STlink v2)(2x10 pins). Both works on the newly soldered STM32C011F6U6TR (320 degree Celcius)
My Successful Setup:
Clock source: Internal HSI 48 Mhz
PA14- Boot0 pin : as SWCLK (did not add any pull-up or pull-down resistor)
PF2 - R\S\T\ pin : as ~Reset (active LOW) pin , this pin is pulled high to 3v3 using 10k resistor.
Thank you so much.