Skip to main content
Associate III
Aug 4, 2026 10:00 PM UTC
Solved

STM32CubeMX2 1.1.1 (Linux) — no silent install, and GUI crashes on startup (reproduced in 4 environments)

Hello,

We're integrating STM32CubeMX2 1.1.1 into a Linux-based development workflow (a VS Code DevContainer running Ubuntu 24.04) for STM32C5xx projects, and have run into two separate blocking issues: the installer has no silent/unattended mode, and once installed, the GUI crashes on startup and never shows a window. Details and everything we've already tried below, in case it saves time on your end.

======================================================================
ISSUE 1 — No silent/unattended install path on Linux

We need to provision STM32CubeMX2 as part of an automated container image build (no interactive session available at build time). We could not find any way to do this:

- Your own docs (STM32CubeMX2 1.0.0 install page) only document the interactive GUI wizard for Linux: chmod +x the installer, run it, click through Welcome -> Configuration -> License -> Installation.
- We tried every CLI flag we could think of or find, including patterns used by OTHER ST installers (e.g. STM32CubeCLT's st-stm32cubeclt_*.deb.sh -- --target ... --quiet --accept, which is a different installer technology — a self-extracting shell wrapper around a .deb — and does not apply to this installer, which is a Tauri/Rust binary).
- Unrecognized flags are silently ignored (no usage/error text is ever printed), which makes it hard to tell whether a flag "isn't a real flag" or "is a real flag that just isn't doing anything yet."
- --guiless IS a real, recognized flag — passing it avoids a GTK-init panic when no window can be shown — but on its own it does nothing observable: no port opens, no files get written to a target directory, process just idles.
- We tried --guiless combined with --target <dir> --quiet --accept (borrowing the CubeCLT installer's flag names, in case they'd been carried over) — still no install, nothing written.

End result: we could only get STM32CubeMX2 installed by running the full interactive GUI wizard once and manually clicking through it, then vendoring the resulting install directory into our own repo/container image so it doesn't need to be repeated per developer/per container rebuild.

Question: is there a documented or undocumented silent/unattended install mode (answers file, env var, hidden CLI flag), and if not, is one planned? A tool that's otherwise clearly meant to be usable in headless/CI/container contexts (it has its own cube mx start --detached --port <port> CLI) seems like an odd fit for a GUI-only installer.

======================================================================
ISSUE 2 — GUI crashes on startup, no window ever maps (reproduced in 4 separate environments)

Once installed, launching the actual STM32CubeMX2 GUI (via cube mx start <project>.ioc2, or directly via the stm32cubemx2 binary) always produces the identical crash, regardless of environment. Console output (same every time):

[Error] Could not initialize contribution TypeError: Cannot read properties of undefined
  (reading 'onChanged')
    at g.initializeEventWatchers (.../lib/frontend/bundle.js:92134:...)
    ...
Opening channel for service path '/services/electron-window'.
[Error] Error: No Cube URI found for project path: <working_area>/<uuid>
[Error] TypeError: Cannot read properties of undefined (reading 'toLowerCase')
[Error] ApplicationProject: Not able to recover hw project information: Error: MCU not found
  on this hw project
(node:PID) UnhandledPromiseRejectionWarning: Error: Cancelled
Backend process exited with code 11   <- seen on some runs, not all

No window is ever created or mapped (confirmed via xpra screenshot — reports "no windows are currently shown" every time), even though the backend process, the pack-manager sync, and the cmsis-scanner service all start up and keep running.

We tried to isolate the cause across FOUR different environments/configurations, changing one variable at a time, and got the identical crash in every single one:

1. Native WSL2/WSLg, host-side (the installer's own GUI wizard actually completes fine and works here — same STM32CubeMX2 build — the crash is specifically in the wizard's INSTALLED
application, not the installer itself).
2. A Linux DevContainer (Docker container, Ubuntu 24.04) with the host's WSLg X11 socket bind-mounted in and DISPLAY forwarded from the host.
3. The same DevContainer, fully self-contained instead — no host display depeebuffer (Xvfb) inside the container, served over HTML5 by xpra, with allGTK/WebKit/Electron runtime deps (libgtk-3-0, libwebkit2gtk-4.1-0, libnss3, libnspr4, etc.) installed.
4. The same DevContainer, swapping Xvfb for a full Xorg server with the xf86-X/RANDR/RENDER support, confirmed via xpra's own log: "OpenGL is supported ondisplay :100") instead of Xvfb's more limited software GL — in case the crash was a GPU-initialization side effect rather than a true logic bug.

We also specifically ruled out two known "silent failure" gotchas we'd found mentioned elsewhere for this tool:
- A stale Electron SingletonLock file (in ~/.config/STM32CubeMX2/) from a preocking a new instance from starting — confirmed present, cleared it, deletedthe whole config directory for a fully clean state, crash reproduced identically.
- A missing D-Bus session bus (many Failed to connect to the bus warnings app real D-Bus session bus via dbus-launch and exported DBUS_SESSION_BUS_ADDRESSbefore launching — crash reproduced identically.

So: not a display/GPU backend issue, not a stale lock file, not a missing D-Bus session. The crash appears to be a genuine bug in the frontend's contribution-initialization code
(initializeEventWatchers), independent of environment.

Environment details for our reproduction:
- STM32CubeMX2 version: 1.1.1 (Linux x64 installer)
- OS: Ubuntu 24.04 (both host-side WSL2/WSLg and inside Docker containers bas
- libwebkit2gtk-4.1: 2.52.3-0ubuntu0.24.04.1 ; libgtk-3: 3.24.41-4ubuntu1.3
- Project: STM32C562RET6 / NUCLEO-C562RE, .ioc2 project file
                                                                                                                                                                              Questions for ST:
1. What does initializeEventWatchers watch, and which service is undefined there? That's the most direct clue we have.                                                        2. Is the eventual backend SIGSEGV (exit code 11, seen on some runs) a conseqbution failure, or an independent fault?
3. Is 1.1.1 known to regress on Linux specifically, and if so is there a workaround or a fixed build we should use instead?                                                   4. Is there a supported way to get a verbose backend log — the wrapper launchd we had to invoke the inner binary directly to see anything at all?
5. Given the tool ships its own headless CLI (cube mx start --detached), is the GUI window expected to be viable at all under a virtual display (Xvfb/Xorg+dummy), or is that configuration simply unsupported/untested on ST's side?

Happy to provide full console logs, installer.json, or anything else useful o

Thank you,

Sara BEN HADJ YAHYA
ST Technical Moderator
Nov 4, 2026 1:19 PM UTC

Hi ​@mani9989, ​@Michael.Angel, ​@Stuart Macdonald ,

I would like to inform you that STM32CubeMX2 is now available through the STM32CubeCLI, providing a command-line option for automated workflows.

For more information, please refer to the Welcome to the STM32CubeCLI topic – start here

Regards,
Sara

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

Sara BEN HADJ YAHYA
ST Technical Moderator
Aug 12, 2026 9:43 AM UTC

Hi ​@mani9989

Thank you for the detailed report,

At the moment, silent installation is not available for STM32CubeMX2. However, this is currently under study and I will keep you posted as soon as there is an update.

Regarding the GUI startup issue, I noticed you are using:

cube mx start <project>.ioc2

This command should be used only if the project has already been created with STM32CubeMX2 and the .ioc2 file already exists.

I would suggest first trying:

cube mx start

and then see whether the GUI starts correctly.

If the issue persists, could you please share a short video or a screenshot showing what happens when you launch the tool?

Regards,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Explorer II
Sep 1, 2026 10:39 PM UTC

I'd like to second @mani9989's request for automated installation options for STM32CubeMX2.

Silent/unattended installation is essential for our workflow, as we need to deploy the tool across multiple machines and integrate it into automated CI/CD pipelines.

 

Sara BEN HADJ YAHYA
ST Technical Moderator
Nov 4, 2026 1:19 PM UTC

Hi ​@mani9989, ​@Michael.Angel, ​@Stuart Macdonald ,

I would like to inform you that STM32CubeMX2 is now available through the STM32CubeCLI, providing a command-line option for automated workflows.

For more information, please refer to the Welcome to the STM32CubeCLI topic – start here

Regards,
Sara

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.