Skip to main content
STackPointer64Best answer
ST Employee
Apr 22, 2026 1:27 PM UTC

Hello @tt2098, and Welcome to ST Community!

This issue has already been reported internally under ticket number CDM0060745, fixed and will be available in the next release. For now, you can use the following option, the only downside is the extra trace signal is pin locked(which will be fixed):

STackPointer64_0-1776864417594.png

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.

3 replies

STackPointer64Best answer
ST Employee
Apr 22, 2026 1:27 PM UTC

Hello @tt2098, and Welcome to ST Community!

This issue has already been reported internally under ticket number CDM0060745, fixed and will be available in the next release. For now, you can use the following option, the only downside is the extra trace signal is pin locked(which will be fixed):

STackPointer64_0-1776864417594.png

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
ST Employee
Apr 22, 2026 1:42 PM UTC

Regarding the PWM configuration, as my colleague mentioned in the other thread, I encourage you to inspect the examples provided in the software package. They show different configurations for different use cases, and each example also includes an IOC2 file that you can inspect and copy.

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Apr 22, 2026 2:27 PM UTC

@tt2098 

As stated by @STackPointer64 your question about PWM example has been answered in this post.

Let's keep this one for the debug settings in CubeMX2.

Need to keep one question per thread.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.