Skip to main content
Associate II
September 24, 2025
Question

STMCubeMX migration ends with successfully imported but nothing is really there.

I have a project with the STM32H753IIT6 with 9 free pins on it all of them labeled and many peripherals configured. I want to migrate to STM32H7R3I8T6 which I understand is the same family of MCU, it should be possible. 

I followed the steps in How to switch from one STM32 to another using STM3... - STMicroelectronics Community

and after selecting the document from where to import I get the "Project is successfully imported. Import RCC : PASS" dialog, but all the configuration remains in default state, nothing has changed. 

I also tried to create a new project with the same MCU as before (STM32H753IIT6) and it was really imported; all pins are there.

Also tried to create a new project with the STM32H753IIT6, assign a few pins, save it and imported this one into the STM32H7R3I8T6 but the result is the same it says it was success, but nothing is changed.

Should I do something different of is this some bug? how can we figure this out?

This topic has been closed for replies.

2 replies

ST Technical Moderator
September 24, 2025

Hello @Alejandro Bizzotto_65856 

Actually, STM32H753IIT6 and STM32H7R3I8T6 are not pin-to-pin compatible, to check the list of pin-to-pin compatible go to Pinout -> List Pinout Compatible MCU and check the list.

Otherwise, I suggest that you refer to this AN Migrating from STM32H730 and STM32H750 to STM32H7Rx/7Sx MCUs - Application note , it may be helpfull.

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
September 29, 2025

Ok, I thought CubeMX will do what it could no matter if they are pin compatible or not. So, there is no automatic or semi-automatic solution to this, right?