Skip to main content
bureau
Associate II
Apr 24, 2026 1:20 PM UTC
Question

STM32N6570-DK: Missing Support for USB PHY Clock Sources

This thread is split from this old discussion

@FBL 


RCC_USBPHY1REFCLKSOURCE_OTGPHY1 and RCC_USBOTGHS1CLKSOURCE_HSE_DIV2 are missing in generated code


I created a simple FSBL application that is jump to the Appli
The Appli is using the same approach (SW solution) like it was implemented inside "Ux_Device_CDC_ACM" example, (it was migrated in to the Appli)
Currently, during debug, I am observing the same issue like it was described before (stuck in USB_CoreReset() during checking the "USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST" )

The solution, that you provided, it looks like it does not working anymore by using the latest Cube_FW and generated compilation errors (no defines for the RCC_USBPHY1REFCLKSOURCE_OTGPHY1 and RCC_USBOTGHS1CLKSOURCE_HSE_DIV2).

Could you please provide a solution (it would be better to see an example) how to solve this issue base on the latest MXCube and STM32CubeIDE versions. Currently it is :

  • STM32CubeIDE_2.1.1 
  • STM32Cube_FW_N6_V1.3.0

 

8 replies

ST Technical Moderator
Apr 26, 2026 4:04 PM UTC

Hi @bureau 

Would you share your firmware ? PHY Reference clock setup is missing for N6 in HAL/LL and MX code generated. The issue is already escalated to dev team under this number CDM0055544 (just for internal use).

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
bureau
bureauAuthor
Associate II
Apr 27, 2026 8:25 AM UTC

@FBL 

By "firmware" --  do you mean a BIN file (FSBL and Appli, or just for the Appli )?

The code that was generated by MxCube:

void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{

 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(pcdHandle->Instance==USB1_OTG_HS)
 {
 /* USER CODE BEGIN USB1_OTG_HS_MspInit 0 */

 /* USER CODE END USB1_OTG_HS_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USBOTGHS1;
 PeriphClkInitStruct.UsbOtgHs1ClockSelection = RCC_USBOTGHS1CLKSOURCE_HSE_DIRECT;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Enable VDDUSB */
 HAL_PWREx_EnableVddUSB();
 /* USB1_OTG_HS clock enable */
 __HAL_RCC_USB1_OTG_HS_CLK_ENABLE();
 __HAL_RCC_USB1_OTG_HS_PHY_CLK_ENABLE();

 /* USB1_OTG_HS interrupt Init */
 HAL_NVIC_SetPriority(USB1_OTG_HS_IRQn, 7, 0);
 HAL_NVIC_EnableIRQ(USB1_OTG_HS_IRQn);
 /* USER CODE BEGIN USB1_OTG_HS_MspInit 1 */

 /* USER CODE END USB1_OTG_HS_MspInit 1 */
 }
}

 

The code that I used during testing

void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{

 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(pcdHandle->Instance==USB1_OTG_HS)
 {
 /* USER CODE BEGIN USB1_OTG_HS_MspInit 0 */

 /* USER CODE END USB1_OTG_HS_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USBOTGHS1;
 PeriphClkInitStruct.UsbOtgHs1ClockSelection = RCC_USBOTGHS1CLKSOURCE_HSE_DIRECT;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Set USB OTG HS PHY1 Reference Clock Source */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USBPHY1;
 PeriphClkInitStruct.UsbPhy1ClockSelection = RCC_USBPHY1CLKSOURCE_HSE_DIRECT;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Enable VDDUSB */
 HAL_PWREx_EnableVddUSB();

 __HAL_RCC_GPIOA_CLK_ENABLE();

 /* Reset USB peripherals and configure the HSE clock */
 RESET_USB_MACRO(); // LL_AHB5_GRP1_ForceReset(0x00800000); \
 __HAL_RCC_USB1_OTG_HS_FORCE_RESET(); \
 __HAL_RCC_USB1_OTG_HS_PHY_FORCE_RESET(); \
 LL_RCC_HSE_SelectHSEDiv2AsDiv2Clock(); \
 LL_AHB5_GRP1_ReleaseReset(0x00800000); \

 __HAL_RCC_USB1_OTG_HS_CLK_ENABLE(); // LL_AHB5_GRP1_EnableClock(LL_AHB5_GRP1_PERIPH_OTG1)

 /* Required few clock cycles before accessing USB PHY Controller Registers */
 HAL_Delay(10);

 USB1_HS_PHYC->USBPHYC_CR &= ~(0x7 << 0x4); // 19.2 MHz
 /*Set the PHY reference clock speed to 24 MHz */
 USB1_HS_PHYC->USBPHYC_CR |= (0x1 << 16) |
 (0x2 << 4) |
 (0x1 << 2) |
 0x1U;
 
 __HAL_RCC_USB1_OTG_HS_PHY_RELEASE_RESET(); // LL_AHB5_GRP1_ReleaseReset(LL_AHB5_GRP1_PERIPH_OTGPHY1);
 HAL_Delay(10);
 __HAL_RCC_USB1_OTG_HS_RELEASE_RESET(); // LL_AHB5_GRP1_ReleaseReset(LL_AHB5_GRP1_PERIPH_OTG1)

 /* Peripheral PHY clock enable */
 __HAL_RCC_USB1_OTG_HS_PHY_CLK_ENABLE(); // LL_AHB5_GRP1_EnableClock(LL_AHB5_GRP1_PERIPH_OTGPHY1)
 
 /* USB1_OTG_HS interrupt Init */
 HAL_NVIC_SetPriority(USB1_OTG_HS_IRQn, 7, 0);
 HAL_NVIC_EnableIRQ(USB1_OTG_HS_IRQn);
 /* USER CODE BEGIN USB1_OTG_HS_MspInit 1 */

 /* USER CODE END USB1_OTG_HS_MspInit 1 */
 }
}

 

 

bureau
bureauAuthor
Associate II
Apr 27, 2026 8:48 AM UTC

@FBL  
@Andrew Neil

As development board I am using NUCLEO-N657X0-Q
https://www.st.com/en/evaluation-tools/nucleo-n657x0-q.html

ST Technical Moderator
Apr 27, 2026 8:48 AM UTC

Hi @bureau 

For the USB PHY reference clock, the current support is still only accessible through low level register access.

So you can just omit this part:

PeriphClkInitStruct.UsbPhy1ClockSelection = RCC_USBPHY1CLKSOURCE_HSE_DIRECT;

As of now, this configuration is not sufficient to fully configure the PHY reference clock. HAL/LL support is missing.

You still need to keep the USB PHY controller register configuration via low level access, and avoid duplication.

/* Set the PHY reference clock speed to 24 MHz */
USB1_HS_PHYC->USBPHYC_CR |= (0x1 << 16) |
 (0x2 << 4) |
 (0x1 << 2) |
 0x1U;

  

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
bureau
bureauAuthor
Associate II
Apr 27, 2026 2:28 PM UTC

Hi @FBL 

By suggested expression:

/* Set the PHY reference clock speed to 24 MHz */
USB1_HS_PHYC->USBPHYC_CR |= (0x1 << 16) |
 (0x2 << 4) |
 (0x1 << 2) |
 0x1U;

afterwards we have 0x03 value inside "FSEL[2:0]: Frequency selection" field which is wrong in my opinion

Explanation:

The default value after the reset, for the "FSEL[2:0]" is 0x01. By applying " |=(0x2 << 4) " --- we have 0x03 which is not defined by the  RM0486 Rev 3
 
 

bureau
bureauAuthor
Associate II
Apr 27, 2026 4:31 PM UTC

@FBL Is it correct that so many registers (see image, marked as yellow) has been cleared after execution of 

 /* Core Soft Reset */
 USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;

 ?Screenshot 2026-04-27 192027.png

Currently, my source code looks like:

void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{

 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(pcdHandle->Instance==USB1_OTG_HS)
 {
 /* USER CODE BEGIN USB1_OTG_HS_MspInit 0 */

 /* USER CODE END USB1_OTG_HS_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USBOTGHS1;
 PeriphClkInitStruct.UsbOtgHs1ClockSelection = RCC_USBOTGHS1CLKSOURCE_HSE_DIRECT_DIV2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Enable VDDUSB */
 HAL_PWREx_EnableVddUSB();
 /* USB1_OTG_HS clock enable */
 __HAL_RCC_USB1_OTG_HS_CLK_ENABLE(); // RCC->AHB5ENSR
 __HAL_RCC_USB1_OTG_HS_PHY_CLK_ENABLE(); // RCC->AHB5ENSR

 /* USB1_OTG_HS interrupt Init */
 HAL_NVIC_SetPriority(USB1_OTG_HS_IRQn, 7, 0);
 HAL_NVIC_EnableIRQ(USB1_OTG_HS_IRQn);
 /* USER CODE BEGIN USB1_OTG_HS_MspInit 1 */
 /* Reset USB peripherals and configure the HSE clock */
 RESET_USB_MACRO();
 
 HAL_Delay(10);
 USB1_HS_PHYC->USBPHYC_CR = 0x10025; // 1: The VBUS valid comparator is powered down. The session valid comparator is ON (default)
 // 010: 24 MHz
 // 1: PHY clocks are off during Suspend and Sleep mode. PLL is off.
 // 1: Retention mode disabled (default)
 
 __HAL_RCC_USB1_OTG_HS_PHY_RELEASE_RESET();

 /* Required few clock cycles before Releasing Reset */
 HAL_Delay(10);

 __HAL_RCC_USB1_OTG_HS_RELEASE_RESET();
 /* USER CODE END USB1_OTG_HS_MspInit 1 */
 }
}

 

ST Technical Moderator
Apr 27, 2026 5:03 PM UTC

Hi @bureau 

I assume it gets cleared after calling reset macro.

RESET_USB_MACRO();

Let me check and will get back to you by tomorrow. I need to check updates with development team. Thank you for your understanding. 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
bureau
bureauAuthor
Associate II
Apr 27, 2026 5:29 PM UTC

@FBL 
No, it is cleared after call of 

/* Core Soft Reset */
 USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;

which is inside 

USB_CoreReset()