Hi @johndoeEngg
The issue occurs when the function releases a timeout while waiting for the USB Core Soft Reset to finish. This timeout happens when the bit CSRST is set in the OTG_GRSTCTL register.
The root cause could be related to the PHY not being properly initialized. After enabling PHY's clock, the sequence should be followed by a delay of 10 cycles before writing core soft reset. This delay is necessary to ensure proper synchronization before resetting USB controller.
/** Initializes the peripherals clock */
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USBOTGHS1;
PeriphClkInitStruct.UsbOtgHs1ClockSelection = RCC_USBPHY1REFCLKSOURCE_HSE_DIRECT;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/** Set USB OTG HS PHY1 Reference Clock Source */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USBPHY1;
PeriphClkInitStruct.UsbPhy1ClockSelection = RCC_USBPHY1REFCLKSOURCE_HSE_DIRECT;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
__HAL_RCC_GPIOA_CLK_ENABLE();
LL_AHB5_GRP1_ForceReset(0x00800000);
__HAL_RCC_USB1_OTG_HS_FORCE_RESET();
__HAL_RCC_USB1_OTG_HS_PHY_FORCE_RESET();
LL_RCC_HSE_SelectHSEDiv2AsDiv2Clock();
LL_AHB5_GRP1_ReleaseReset(0x00800000);
/* Peripheral clock enable */
__HAL_RCC_USB1_OTG_HS_CLK_ENABLE();
/* Required few clock cycles before accessing USB PHY Controller Registers */
HAL_Delay(1);
USB1_HS_PHYC->USBPHYC_CR &= ~(0x7 << 0x4);
/*Set the PHY reference clock speed to 24 MHz */
USB1_HS_PHYC->USBPHYC_CR |= (0x1 << 16) |
(0x2 << 4) |
(0x1 << 2) |
0x1U;
__HAL_RCC_USB1_OTG_HS_PHY_RELEASE_RESET();
/* Required few clock cycles before Releasing Reset */
HAL_Delay(1);
__HAL_RCC_USB1_OTG_HS_RELEASE_RESET();
/* Peripheral PHY clock enable */
__HAL_RCC_USB1_OTG_HS_PHY_CLK_ENABLE();
HAL_Delay(1) introduced here is dependent on CPU frequency and not reliable. You can insert __NOP() to ensure that the delay is consistent. The volatile keyword ensures that the loop is not optimized away by the compiler.
/* Required few clock cycles before accessing USB PHY Controller Registers */
for (volatile uint32_t i = 0; i < 10; i++) {
__NOP(); // No Operation instruction to create a delay
}
To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL