Skip to main content
Till Rachow
Associate III
Aug 10, 2018 7:22 AM UTC
Solved

STM32CubeMX deletes Src folder..

Hi,

When I am generating Code with CubeMX, it will delete my complete Src folder. I always have to recover it. For that reason it will also not generate any new c files once i add a new peripheral.

Tried this on Mac and Windows with latest CubeMx version (4.26.1) and i get the same behaviour in both.

Can anybody help?

Thanks

This topic has been closed for replies.
Mohamed Mansouri
Mohamed MansouriBest answer
Visitor II
Sep 5, 2018 7:38 AM UTC

Hi,

Thanks for your feedback,

I confirm its a bug, and it will be fixed in next CubeMX version 4.27.0,

Please feel free to contact me for further information,

Best regards,

Mohamed

24 replies

Till Rachow
Associate III
Aug 10, 2018 7:40 AM UTC

Seems to be a bug in STM32Cube FW_L4 V1.11.0

In STM32Cube FW_L4 V1.12.0 it works fine. Unfortunately i cannot update my project right now, so if STM32Cube FW_L4 V1.11.0 would work, i would be more than happy..

ST Technical Moderator
Aug 10, 2018 11:22 AM UTC

Hello @Till Rachow​ ,

Your project works fine with STM32Cube FW_L4 V1.12.0 ! So, why do you need to work with previous version of CubeL4?

Can you please share your ioc file to check your issue.

With Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Takemasa
Associate III
Aug 19, 2018 10:52 AM UTC

Hello

I have same problem :

  • OS : Ubuntu 16.04 LTS
  • Tool : CubeMX ver 4.26.1
  • Target : STM32L152RE​
  • Tested firmware : STM32Cube MCU Package for STM32L1 series ver 1.7.0, 1.8.0, 1.8.1

For each time I generate code for a target, CubeMx deletes the Src folder. I found this problem today. Two months ago, it was working without problem. 

Any workaround for this problem?

Regards,

Till Rachow
Associate III
Aug 20, 2018 8:41 AM UTC

Hi @Imen DAHMEN​ ,

In the current project state I can't afford to introduce any possible changes or errors by upgrading the library version.

Regards,

Till

cgarrett
Visitor II
Aug 21, 2018 9:21 PM UTC

I have the same issue with Cube v4.26.1 and F3 HAL v1.09.0. Src folder gets entirely deleted when regenerating, including any user files. My only workaround was to switch to advanced and restructure the project using the generated 'Core' folder. Not sure if F3 HAL v1.10.0 also has this issue, but I am unable to attempt at this time as there are significant changes to the HAL API that would require a code restructure.

Schmid.M.
Associate III
Aug 22, 2018 9:17 AM UTC

We have te same bug here with Cube v4.26.1 and the L0 lib , this makes the tool completely unusable. older cube versions are not available for download anymore, so we are stuck. Hoping for a bugfixed version to be released soon.

Takemasa
Associate III
Aug 26, 2018 3:32 AM UTC

Hi

Attached IOC file is problematic one.

  • OS : Ubuntu 16.04 LTS
  • Tool : CubeMX ver 4.26.1
  • Target : STM32F091RC​

ST Technical Moderator
Aug 27, 2018 7:56 AM UTC

Hello All,

I raised your feedback internally to our CubeMx team for investigation, and we will come back to you as soon as possible.

Thank you for your contribution and comments.

With Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Mohamed Mansouri
Mohamed MansouriBest answer
Visitor II
Sep 5, 2018 7:38 AM UTC

Hi,

Thanks for your feedback,

I confirm its a bug, and it will be fixed in next CubeMX version 4.27.0,

Please feel free to contact me for further information,

Best regards,

Mohamed

Brian Rau
Associate III
Sep 6, 2018 1:00 PM UTC

Mohamed, any idea WHEN the 4.27.0 release will be? This is holding up software development for many of us!