A
Anonymous
Aug 13, 2021 2:09 PM UTC
Question
Problem with CUBEMX 6.3 and CUBE F4 V26.2
- 15 replies
- 2364 views
Hello dear Engineers,
Before this upgrade(downgrade?????), I was able to use FREERTOS successfully. The main procedure was to change the time base from SYSTICK to TIM1 and then everything was working. Now in this upgrade even without FREERTOS, when the time base is set to any timer but SYSTICK, it gets stuck at HAL_Init();.
The project is attached for further analysis. The board is a custom board.
sincerely yours