Skip to main content
Aug 13, 2021 2:09 PM UTC
Question

Problem with CUBEMX 6.3 and CUBE F4 V26.2

Hello dear Engineers,

Before this upgrade(downgrade?????), I was able to use FREERTOS successfully. The main procedure was to change the time base from SYSTICK to TIM1 and then everything was working. Now in this upgrade even without FREERTOS, when the time base is set to any timer but SYSTICK, it gets stuck at  HAL_Init();.

The project is attached for further analysis. The board is a custom board.

sincerely yours

This topic has been closed for replies.

15 replies

Mar 15, 2022 4:49 PM UTC

Dear @Khouloud OTHMAN​ 

beachmiles has a solution to this problem and worked for me.

https://github.com/STMicroelectronics/STM32CubeF4/issues/113