Skip to main content
Associate II
October 3, 2025
Solved

OCTOSPI Multiplexed setting gone after IDE/MX update

This morning I updated my CubeIDE to 1.19 from 1.18.  I assume MX updated too... don't know how to check the MX version.

After updating and then opening and migrating my project to 1.19, my OCTOSPI settings and the "octospi.c" file were gone.  When I try to set things back the way they were in 1.18, there is no longer an option for "Quad SPI -- MULTIPLEXED --".  My circuit has a flash IC and a RAM IC sharing the bus on Data [3:0] (Port1 IO[3:0] -- MULTIPLEXED --).  This has been working when using IDE 1.18, but now I'm stuck.

How do I setup the new MX to multiplex OCTOPSPI1 and OCTOSPI2 ?

Souhaib MAZHOUDBest answer
ST Technical Moderator
October 6, 2025

Hello @SJR1 

The fix will be implemented in the next release of STM32CubeMX. Unfortunately, the only workaround for the moment is to generate your required Quad SPI code using an older version of CubeMX (6.14.1 or STM32CubeIDE 1.18.1) and then copy the generated code (MX_OCTOSPI1_Init) and files into your new project.

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

6 replies

ST Technical Moderator
October 3, 2025

Hello @SJR1 

This is a known issue that has already been discussed in this thread, and it will be resolved as soon as possible.
Thank you.

KR,

Souhaib

 

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
SJR1Author
Associate II
October 3, 2025

ok.. now I see this:

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-version-1-19-0-quadspi-unavailable-on-stm32h723zg/td-p/821969

What is the status of the ticket?  What is the work around? 

Souhaib MAZHOUDBest answer
ST Technical Moderator
October 6, 2025

Hello @SJR1 

The fix will be implemented in the next release of STM32CubeMX. Unfortunately, the only workaround for the moment is to generate your required Quad SPI code using an older version of CubeMX (6.14.1 or STM32CubeIDE 1.18.1) and then copy the generated code (MX_OCTOSPI1_Init) and files into your new project.

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
SJR1Author
Associate II
December 4, 2025

The errata from the new IDE and MX version do NOT mention this.  I'll assume this is still NOT SOLVED!!!  Why is it marked as "Solved"?

SJR1Author
Associate II
November 21, 2025

Looks like STM32CubeIde 2.00 is out.. is it fixed?