Skip to main content
MHoll.2
Senior III
November 4, 2025
Solved

MX_TouchGFX_PreOSInit() called before I can init my external (QSPI) Flash

The STM32CubeMX generated main.c has the function MX_TouchGFX_PreOSInit() called directly after the MX_xxx_Init() functions, before I can insert my External Flash Initialisation (in /* USER CODE BEGIN 2 */).

This prevents the use of the External Flash for the TextFlashSection defined by TouchGFX.

It would be better to call MX_TouchGFX_PreOSInit() immediatly before MX_xxx_Init() (in my case  MX_ThreadX_Init()).

Souhaib MAZHOUDBest answer
ST Technical Moderator
November 7, 2025

Hello @MHoll.2 

As my understanding you can initialize the External flash inside the MX_OCTOSPI1_Init() (/* USER CODE BEGIN OCTOSPI1_Init 2 */). This will ensure that the external flash is initialized before the call of MX_TouchGFX_init.

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
November 4, 2025

Hello @MHoll.2 

What MCU are you using? Or could you provide your IOC in order to investigate further the issue.

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
MHoll.2
MHoll.2Author
Senior III
November 4, 2025

Hi Souhaib,

I'm using the STM32H725IEK.

Attached a small example ioc file that generates

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MPU Configuration--------------------------------------------------------*/
 MPU_Config();

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_OCTOSPI1_Init();
 /* Call PreOsInit function */
 MX_TouchGFX_PreOSInit();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 MX_ThreadX_Init();

 /* We should never get here as control is now taken by the scheduler */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

  I'm using STMCubeIDE 1.18.1, beause of  this problem:  https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-19-0-problem-migrating-octospi2-stm32h730-from-1/td-p/819983

 

Martin

Souhaib MAZHOUDBest answer
ST Technical Moderator
November 7, 2025

Hello @MHoll.2 

As my understanding you can initialize the External flash inside the MX_OCTOSPI1_Init() (/* USER CODE BEGIN OCTOSPI1_Init 2 */). This will ensure that the external flash is initialized before the call of MX_TouchGFX_init.

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.