Skip to main content
Associate
September 18, 2025
Solved

How to setup hfmpi2c1 using STM32F446

  • September 18, 2025
  • 3 replies
  • 916 views

I have enable the hfmpi2c1 in STM32CubeMX tools, but I can find the 

FMPI2C_HandleTypeDef is undefined in the source code.
 
Do we have a demo code to show how to setup and use hfmpi2c1.
 
It's very confuse that the F446 only have one Fast Plus Mode IIC interface.

Lding2025_0-1758166731293.pngLding2025_1-1758166779567.pngLding2025_2-1758166817354.png

 

Best answer by mƎALLEm

Hello and welcome to the ST community,

I didn't really understood the issue.

I just generated a code with the latest CubeMx version 6.15.0 with I2C in Fast mode + and FMPI2C_HandleTypeDef is defined. 

In the main, this is what I get:

/* Private variables ---------------------------------------------------------*/
FMPI2C_HandleTypeDef hfmpi2c1;

 If I compile the project I don't have any error.

This is my configuration:

mALLEm_0-1758201152756.png

For your last question, I didn't really understand the meaning! Do you mean the number of instances available on that device? if yes, this information is available in the datasheet:

mALLEm_1-1758201334243.png

4xI2C instances are available on that device, only I2C1 features Fast mode/+.

 

 

 

3 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 18, 2025

Hello and welcome to the ST community,

I didn't really understood the issue.

I just generated a code with the latest CubeMx version 6.15.0 with I2C in Fast mode + and FMPI2C_HandleTypeDef is defined. 

In the main, this is what I get:

/* Private variables ---------------------------------------------------------*/
FMPI2C_HandleTypeDef hfmpi2c1;

 If I compile the project I don't have any error.

This is my configuration:

mALLEm_0-1758201152756.png

For your last question, I didn't really understand the meaning! Do you mean the number of instances available on that device? if yes, this information is available in the datasheet:

mALLEm_1-1758201334243.png

4xI2C instances are available on that device, only I2C1 features Fast mode/+.

 

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Lding2025Author
Associate
November 10, 2025

do you have a demo code to show how to read a device id with hfmpi2c1.

mƎALLEm
ST Technical Moderator
November 10, 2025

@Lding2025 wrote:

do you have a demo code to show how to read a device id with hfmpi2c1.


You need to ask that question in STM32 MCUs Embedded software forum.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.