Skip to main content
Visitor II
July 13, 2024
Question

error:"This feature requires internet connection"

  屏幕截图 2024-07-13 134732.pngWhen I try to log in to my ST account in STM32CubeMX, it sends me an error message that says, 'This feature requires an internet connection.' However, my internet connection is working well, and I can use other browsers to surf the internet normally.

How can I solve this problem?

This topic has been closed for replies.

3 replies

Semer CHERNI
ST Employee
July 15, 2024

Hello @Pea 

First let me thank you for posting.

Are you using a proxy with your network?

If it's the case set it up in the "Updater settings". Check this article for more details :How to set the network connection parameters for S... - STMicroelectronics Community

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Explorer
July 23, 2025

What if I'm not using a proxy?!?  I'm getting that same error message with the latest STM32CubeIDE (1.19.0) running on Linux in a VM.  The VM can access the Internet, but STM32CubeIDE keeps asking me to set my Network connection.  I get "This feature requires Internet connection...", then a few seconds later, I get "Authentication Error Manager" - "Connection lost...".

Why is this so hard when I've not using a proxy???

Patrick

Pavel A.
July 26, 2025

Then something weird is going with your VM, or some "security", "compliance", "EDR" trouble-ware in your network?

Can you provide more info to reproduce?

* What is the host OS

* What is the guest OS

* Which hypervisor? Type of virtual network: bridged or NAT?