Skip to main content
Visitor II
August 24, 2025
Question

CubeMX 6.15 Not Generating .ld File for Dual-Core STM32H755 Project (Toolchain: STM32CubeIDE)

Hello everyone, I'm creating a TIM3-based project using CubeMX. I'm using the Nucleo-H755ZI development board, which features the STM32H755ZITx dual-core MCU.I've completed all the necessary configurations—GPIO settings, TIM settings, SYS, and PROJECT settings. However, when I click "Generate Code," it creates the main.c file but does not generate the xxx_FLASH.ld linker script file. My selected Toolchain is STM32CubeIDE. I'm using CubeMX version 6.15 and CubeIDE version 1.19.

Does anyone have any idea what might be causing this issue?

 

6 replies

TDK
August 24, 2025

Include the IOC file you're having trouble with.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
August 25, 2025

Hello @TufanHan ,

 

Let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
August 25, 2025

Hello @TufanHan ,

 

Further to your comment, I was not able to reproduce your request.

Could you provide please your Ioc.File.

MahmoudBenRomdhane_0-1756137234123.png

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
August 26, 2025

If you are on Linux (or MacOS on a case sensitive disk), you might have the same issue as i just reported here?
https://community.st.com/t5/stm32cubemx-mcus/wrong-file-name-for-linker-script/m-p/834008/thread-id/33307

Visitor II
December 9, 2025

I have same problem. So, I updated 6.16.0, but still ld file wasn't generated. Did you fixed it? 

ST Technical Moderator
December 10, 2025

Hello @LXIV ,

 

Could you provide please which Operating System you are using.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.