Skip to main content
Associate II
August 26, 2025
Question

Wrong file name for linker script

  • August 26, 2025
  • 1 reply
  • 422 views

When generating code for Makefile, the MacOS version 6.15 succeeds while the Linux version 6.15 fails.

I have the same version of firmware packages installed on both OS.

MacOS STM32CubeMX produce this following snippet in the Makefile

#######################################
# LDFLAGS
#######################################
# link script
LDSCRIPT = STM32U5a5xx_FLASH.ld

and do copy the correct file to the project directory. 

However, the Linux version fail to define linker script file and does not copy required script to the project folder. 

#######################################
# LDFLAGS
#######################################
# link script
LDSCRIPT = 

The log explains why, the file does not exists.

No such linker file: /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5a5xx_FLASH.ld
No such linker file: /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5a5xx_RAM.ld

However, it appears the files exists, but has different case, like so (note "U5A5" not "U5a5"):

mike@mabox:~$ ll /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5A5xx_*
-rw-r--r-- 1 mike mike 4959 Aug 27 01:25 /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5A5xx_FLASH.ld
-rw-r--r-- 1 mike mike 5123 Aug 27 01:25 /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5A5xx_FLASH_ns.ld
-rw-r--r-- 1 mike mike 5347 Aug 27 01:25 /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5A5xx_FLASH_s.ld
-rw-r--r-- 1 mike mike 4859 Aug 27 01:25 /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5A5xx_RAM.ld
-rw-r--r-- 1 mike mike 4941 Aug 27 01:25 /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5A5xx_RAM_ns.ld
-rw-r--r-- 1 mike mike 5157 Aug 27 01:25 /home/mike/STM32Cube/Repository//STM32Cube_FW_U5_V1.8.0//Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker/STM32U5A5xx_RAM_s.ld

Likely, this works on Windows and MacOS disks that are not case sensitive, but not on Linux.

A workaround that do work is to create symbolic links, like so:

$ cd ~/STM32Cube/Repository/STM32Cube_FW_U5_V1.8.0/Drivers/CMSIS/Device/ST/STM32U5xx/Source/Templates/gcc/linker
$ ln -s STM32U5A5xx_FLASH.ld STM32U5a5xx_FLASH.ld
$ ln -s STM32U5A5xx_RAM.ld STM32U5a5xx_RAM.ld

 After this, Makefile is correctly generated and the linker script files are copied to the project directory.

This topic has been closed for replies.

1 reply

Ghofrane GSOURI
ST Technical Moderator
August 27, 2025

Hello @MikeStrom 

Thank you very much for your detailed description.

The issue has been escalated to our development team for resolution.
The internal ticket number is 216370.

I will keep you updated on any progress

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.