Skip to main content
AOgra.1
Visitor II
Jan 16, 2022 11:35 PM UTC
Question

What is the correct setup to use multiple st-links for debugging with stm32cube ide?

I'm working on a project to connect multiple stm32-boards using the CAN-bus.

So I opened two instances of the ide and connected 2 boards with 2 st-links.

When I tried to setup the 2nd st-link for debug, I received an unknown error from the GDB-server.

Please help, as I don't want to use multiple computers for that project.

Regards

Andreas

This topic has been closed for replies.

5 replies

Markus GIRDLAND
ST Employee
Jan 17, 2022 10:30 AM UTC

Hello there!

You only need to run one instance of STM32CubeiDE regardless of the number of boards you debug in parallel.

You will need to specify the serial number of the ST-Link in your debug configuration (debugger tab) and might need to change port numbers so they don't collide with each other.

You can find more information about how to set it up in the STM32CubeIDE User Manual chapter 3.6.3.

PR.10
Associate III
May 18, 2022 8:59 PM UTC

Thanks for the answer. I run in to the same error. From the form layout I assumed the port is relevant only for remote server selection, but it is it applies to local host too and changing it solved the conflict. In GUI It would would be more intuitive to put host name where port number label is now and port number move away from radio button line. (Version: 1.9.0)

Graduate II
Apr 22, 2025 1:16 AM UTC

I think the very similar question and answer was already posted here. Check that post, and it would be helpful.

https://community.st.com/t5/stm32cubeide-mcus/stmcube-ide-can-we-use-two-debug-window-at-time/td-p/179884