Skip to main content
Associate II
Aug 22, 2026 5:02 PM UTC
Solved

Unable to import examples which stm32 provided for reference .

d8abeb2d-1160-0047-a792-2fac2b402929.png

Above image you can see in toolchain option STM32IDE is disable . also i am facimng issure i =n import examples which stm32 provided for reference . you can also refer my shared video.

ST Technical Moderator
Aug 22, 2026 5:10 PM UTC

Hello  @shreya_awati  

Open STM32CubeIDE 2.1.1.

Right Click on File, then click on STM32 Project Create/Import : 

448e8a5e-3a48-efa1-cec1-e356b8c07034.png

03455759-5907-b8ba-de56-10ffd753f4b4.png

d7c14fa7-48fe-6d6e-7222-89f2edfd2846.png

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

18 replies

Associate II
Aug 22, 2026 5:11 PM UTC

For only GPIO example is working


other not able to import 

/home/sawati/STM32Cube/Repository/STM32Cube_FW_F7_V1.17.4/Projects/STM32F746ZG-Nucleo/Examples/ADC/ADC_RegularConversion_Interrupt/SW4STM32/STM32746ZG_Nucleo

9b942b1b-76c7-0375-c91e-37e2ea6b383b.png

 

Associate II
Aug 22, 2026 5:11 PM UTC

I import GPIO toggle example , after that i am trying to import another example but it is not showing build option . directly it is showing run option . Then i deleted gpio example and tried to import another example then is is showing build option . 

how can i resolve this issue ??

Pavel A.
Aug 24, 2026 4:33 AM UTC

This is because both ADC and GPIO projects have the same name “STM32746ZG_Nucleo”.

Eclipse doesn’t allow two projects with same name in one workspace. Rename the other project or create a new empty workspace for the DMA.