Skip to main content
Associate II
Aug 22, 2026 5:02 PM UTC
Solved

Unable to import examples which stm32 provided for reference .

d8abeb2d-1160-0047-a792-2fac2b402929.png

Above image you can see in toolchain option STM32IDE is disable . also i am facimng issure i =n import examples which stm32 provided for reference . you can also refer my shared video.

ST Technical Moderator
Aug 22, 2026 5:10 PM UTC

Hello  @shreya_awati  

Open STM32CubeIDE 2.1.1.

Right Click on File, then click on STM32 Project Create/Import : 

448e8a5e-3a48-efa1-cec1-e356b8c07034.png

03455759-5907-b8ba-de56-10ffd753f4b4.png

d7c14fa7-48fe-6d6e-7222-89f2edfd2846.png

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

18 replies

TDK
Aug 22, 2026 5:06 PM UTC

Yeah, it doesn't just work for the F7 series. Seems ST haven't taken the effort to update the example selector for that series and the SW4STM32 conversion has apparently broken over time. Shrug. The files are all there. You could create a new project for that chip and copy them over, but it would take some effort.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Aug 22, 2026 5:06 PM UTC

 

Use the Example Selector in STM32CubeMX for the easiest way to load examples.

> another example

Be more specific.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
Aug 22, 2026 5:09 PM UTC

0e3f3e34-0bed-7955-b3e6-40fd6851a05e.png



which path i can select for "Install project directory" . what is meant we are import examples from software package examples or it is location for store example .

For open with option i am not able to see STM32IDE , only below options are available.
SW4STM32
EWARM
MDK-ARM
Explorer

. please give me steps from scratch.


 

Pavel A.
Aug 22, 2026 5:10 PM UTC

> which path i can select for "Install project directory" . what is meant we are import examples from software package examples or it is location for store example .

It is where you want to create your copy of the project. The original (source) is in the MCU firmware package in the Cube "repository".  [To remind - the project directory path must NOT contain spaces and weird characters in any subdirectory.]

If the CubeIDE option is not available: select SW4STM32. After CubeMX finishes its magic, use CubeIDE to import the project with conversion from SW4STM32 format (they both are different flavors of Eclipse CDT).

 

Pavel A.
Aug 22, 2026 5:07 PM UTC

Try exporting for SW4STM32, then convert by CubeIDE project import.

dcadc1db-9785-1d7b-c683-9b31acc4cf15.png

 

 

Associate II
Aug 22, 2026 5:09 PM UTC

Can you please provide steps from scratch . 

 

Associate II
Aug 22, 2026 5:10 PM UTC

which version of IDE you using . i am using MX is 6.17.0 and IDE is Version: 2.1.1 
I am importing package from MX for F7 latest . In image you can see package is successfully installed . 

Please tell me in detail steps how can i import .

44937e2c-8029-ac6d-5ff2-fcd57fc141ee.png

 

Associate II
Aug 22, 2026 5:10 PM UTC

7924f2f5-1f68-eb7e-7d10-80cfe16c5d12.png

git this error.

 

Pavel A.
Aug 22, 2026 5:10 PM UTC

Hmm. As  @TDK commented, conversion from SW4STM32 is not perfect. Looks like you have to check and fix include paths and other project settings after conversion. This may be, unfortunately, too confusing for a beginner, and you may use some help.

For a simple project such as GPIO blinky, better create a new project with CubeMX (or CubeIDE 1.9) or find existing example for CubeIDE.

ST Technical Moderator
Aug 22, 2026 5:10 PM UTC

Hello  @shreya_awati  

Open STM32CubeIDE 2.1.1.

Right Click on File, then click on STM32 Project Create/Import : 

448e8a5e-3a48-efa1-cec1-e356b8c07034.png

03455759-5907-b8ba-de56-10ffd753f4b4.png

d7c14fa7-48fe-6d6e-7222-89f2edfd2846.png

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Aug 22, 2026 5:11 PM UTC

Its working fine.

Thanks 

Associate II
Aug 22, 2026 5:11 PM UTC

i want to use other examples not gpio . i didnt study ADC and other components so i need imported examples for reference . above you shared "use some help" link not useful for me .

please help me find out solutions

Pavel A.
Aug 22, 2026 5:11 PM UTC

AI tool such as Github Copilot or Claude Code can be asked to fix include paths in CubeIDE project.