Skip to main content
Visitor II
Jul 22, 2025 2:10 PM UTC
Question

Unable to Create STM32 Project – "Fix the highlighted errors and try again" Issue

Dear STM32 Support Team,

I am trying to create a new project in STM32CubeIDE, but I encounter a few issues. First, I cannot select the "STM32Cube" option under the Targeted Project Type section when starting a new project.

To work around this, I tried generating code through STM32CubeMX after completing my .ioc configurations. While the code is transferred to STM32CubeIDE, many essential files are missing, and the project does not build or run properly.

Additionally, STM32CubeIDE displays an error message saying: "Fix the highlighted errors and try again." However, I cannot identify what these errors refer to, as nothing is clearly highlighted.

I am using the latest version of STM32CubeIDE, and I have already uninstalled and reinstalled the software, but the problem still persists.

Could you please help me resolve this issue?

Best regards,
Emre MERCAN

Emremercancoder_0-1753193383881.png

 

This topic has been closed for replies.

2 replies

TDK
Jul 22, 2025 7:14 PM UTC

This is the error:

TDK_0-1753211633319.png

 

Put in a name for the project to correct this error.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Jul 23, 2025 2:03 PM UTC

As @TDK  said, you need to enter a project name.

But also see this pinned post about a known issue with the 'STM32CubeIDE' Project Type being greyed-out:

STM32CubeIDE STM32Cube project creation issue

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.