Skip to main content
Senior
March 20, 2024
Question

target is not responding issue

Hi,

When I flash my code, I encounter the issue below. I have unplugged the cable of the board, but that didnt work.

Could you please help me resolve ?

 

 

STMicroelectronics ST-LINK GDB server. Version 7.5.0

Copyright (c) 2023, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.15.0

-------------------------------------------------------------------

 

 

 

Log output file: C:\Users\.....\AppData\Local\Temp\STM32CubeProgrammer_a09028.log

ST-LINK SN : 066DFF575377524867051414

ST-LINK FW : V2J43M28

Board : STM32F4DISCOVERY

Voltage : 4.08V

SWD freq : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x413

Revision ID : Rev Y

Device name : STM32F405xx/F407xx/F415xx/F417xx

Flash size : 1 MBytes (default)

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0x91

 

 

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a09028.srec

File : ST-LINK_GDB_server_a09028.srec

Size : 10.00 KB

Address : 0x08000000

 

 

Erasing memory corresponding to segment 0:

Erasing internal memory sector 0

Download in Progress:

 

 

File download complete

Time elapsed during download operation: 00:00:00.459

 

 

 

Verifying ...

 

 

 

 

Download verified successfully

 

 

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Shutting down...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

 

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
March 20, 2024

Hello @demir 

I suggest you to take a look at those two posts (post 1 and post 2). They should solve your issue.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
demirAuthor
Senior
March 20, 2024

Surprisingly, everything got back to normal after I closed CUBE IDE and created new project.

Thanks for your reply.