Skip to main content
PTiha
Associate III
July 3, 2020
Question

Support from ST is dead?

I first reported bugs related to the STM32CubeIDE SWV viewer on February 25th. No ST employees responded to it or were considered.

I also opened a topic for almost three weeks, but the result is the same: they don't even try to deal with the topic.

They seem to be trying almost exclusively to solve trivial problems that can be easily solved.

I started dealing with STM32 microcontrollers a year and a half ago, with great enthusiasm. One of the key factors was the great support.

This is exactly the biggest disappointment for me right now.

This topic has been closed for replies.

13 replies

S.Ma
Principal
July 5, 2020

Well, my 2 cents would say that if it's open source, better test with the least performing compiler (IAR to GCC caused at no optimisation debug level malfunction due to SPI and EXTI Timings between MCUs (Master and Slaves). So on compiler side, there is value to make a code work with the less performant one.

I can't comment on IDE under the hood technology, however, would we say that Android developpers IDE evolution could be inspirational? (was Eclipse in 2015, now IntelliJ... still?)

Luca1
Associate III
July 6, 2020

I agree with you that the Keil and Iar IDE have an "old" UI aspect, but they are more powerfull (and more expensive) than eclipse IDE.

I haven't particular problem with the IDE,, the problem for me arise about the logic of the ST software. It can be usefull, but is too much rigid. Or you use the ST software philosophy or not use it, but if you want to use it you need to learn how to use it.. and this is not easy..

On the other hands, if you want to learn how to programm the ST microcontroller, is a bad idea to use the ST software. In this case the IDE can't help. It generate the code, or not generate nothing, so if you want to learn you need to manually configure the project and after to configure the microcontroller... 

The life is fuzzy, but if you use the ST the life is black or withe! Poor me! :)