Skip to main content
Associate III
Mar 7, 2026 12:44 PM UTC
Solved

STM32H7B3I-EVAL – CubeIDE not opening .ioc; missing MCU package manager

Hello STMCommunity,

I am a beginner working with the STM32H7B3I-EVAL evaluation board (MCU: STM32H7B3LIH6Q) and I am currently setting up my development environment on Ubuntu 24.04 Linux.

I installed STM32CubeIDE using the following installer:

st-stm32cubeide_2.1.0_27993_20260219_1630_amd64.deb_bundle.sh. zip

However I am facing several issues during setup and project creation.

Problems I am facin

  1. Embedded Software Package Manager missing

    • I cannot find the option: Help → Manage Embedded Software Packages

    • The STM32H7 firmware package does not appear to be installed.

  2. Unable to create a proper project

    • When creating a new STM32 project for STM32H7B3I-EVAL, the project builds incorrectly and sometimes shows: make: *** No rule to make target 'all'. Stop.

    • The expected firmware output files (.elf, .hex, .bin) are not generated.

  3. CubeMX integration problem

    • It appears that STM32CubeMX is not properly integrated with STM32CubeIDE on my Linux system.

  4. .ioc file does not open

    • When I double-click the .ioc file in STM32CubeIDE, the CubeMX configuration window does not open.

  5. Please Provide me Existing Demo Codes:  For this Board also provide Demo Code which is Flashed in Board Firmware version is  V1.0.1 give me correct code. Provide me LED, ADC, Other periphearal Demo codes separately I am using Linux Ubuntu 24.04.3 LTS.
  6. WiFi module issues

    • In  Existing Demo Code  The board includes a WiFi module Available WiFi Show I use correct password but unable to connect wifi , but I am not able to find working demo examples or documentation explaining how to test or use the WiFi functionality on this evaluation board.                                                                                                                                                                                                                         Thank You.

       

       

TDK
TDKBest answer
Mar 7, 2026 2:23 PM UTC

Use the standalone STM32CubeMX program to create projects. This functionality has been removed starting with STM32CubeIDE v2.0.

STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."

4 replies

TDK
TDKBest answer
Mar 7, 2026 2:23 PM UTC

Use the standalone STM32CubeMX program to create projects. This functionality has been removed starting with STM32CubeIDE v2.0.

STM32CubeIDE 2.0 release - early heads-up! - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate III
Mar 9, 2026 7:31 AM UTC

 

Hello STMCommunity,

I am a beginner working with the STM32H7B3I-EVAL evaluation board (MCU: STM32H7B3LIH6Q) and I am currently setting up my development environment on Ubuntu 24.04 Linux.

I installed STM32CubeIDE using the following installer:

st-stm32cubeide_1.18.0_24413_20250227_1633_amd64.sh.zip

Problems I am facin

  1. Please Provide me Existing Demo Codes:  For this Board also provide Demo Code which is Flashed in Board Firmware version is  V1.0.1 give me correct code. Provide me LED, ADC, Other periphearal Demo codes separately I am using Linux Ubuntu 24.04.3 LTS.
  2. WiFi module issues

    • In  Existing Demo Code  The board includes a WiFi module Available WiFi Show I use correct password but unable to connect wifi , but I am not able to find working demo examples or documentation explaining how to test or use the WiFi functionality on this evaluation board.                                                                                                                                                                                                                         Thank You.

Vijaya
Andrew Neil
Super User
Mar 12, 2026 10:05 AM UTC

You have a separate thread on that question: STM32H7B3I-EVAL: Need demo codes, Wi-Fi support; Ubuntu 24.04

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Jun 15, 2026 6:46 AM UTC

Title: Is it possible to add a custom board to STM32CubeMX Board Selector?

Hello ST Community,

I am working on a custom STM32-based board and would like to know whether STM32CubeMX provides any official feature to add our own custom board to the Board Selector, similar to ST Discovery, Nucleo, or Evaluation boards.

My requirement is that when creating a new project, I should be able to select my custom board and automatically load the default settings such as MCU, pin configuration, clock settings, peripherals, and middleware from a predefined .ioc file.

Is this feature officially supported by STM32CubeMX, or is the recommended method to manually create and reuse a base .ioc file for each custom board?

Thank you.

Vijaya