Associate
Feb 14, 2025 9:21 AM UTC
Question
STM32cubeIDE cannot use ST-LinkV2 run/debug software
- 3 replies
- 1073 views
When I click run to program, it pops-up an error, see attached error picture:
I checked the configure setting, it shows in the attached files.
and the IDE log:
Log output file: C:\Users\Johnson\AppData\Local\Temp\STM32CubeProgrammer_a14788.log
ST-LINK SN : 361F0D14C216303030303032
ST-LINK FW : V2J45S7
Board : --
Voltage : 3.16V
Error: ST-LINK error (DEV_TARGET_RESET_ERR)
Encountered Error when opening C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.400.202404281720\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
I don't know what had happen. I can use STE32CubeProgrammer flash the firmware success. But can not debug with STM32cubeIDE.