Skip to main content
Visitor II
Jul 23, 2025 1:40 PM UTC
Question

STM32CubeIDE CAN examples for Nucleo-L476RG

Hello all.

Im starting to work with the Nucleo L476RG board and am now at the stage i would like to bring up the CAN bus. I haven noticed there are CAN bus examples available for other Nucleo baords but not in the current STM32Cube_FW_L4_V1.18.1 for the L476. Is this available or been ported to the L476?

Many thanks
Rich

This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
Aug 1, 2025 10:00 AM UTC

Hello @Rich_P and welcome to the community;

 

I recommend you referring to these examples and get inspired to configure CAN bus:

- STM32CubeL4/Projects/STM32L476G-EVAL/Examples/CAN/CAN_Networking at master · STMicroelectronics/STM32CubeL4 · GitHub  This example runs on STM32L476xx devices and it has been tested with STM32L476G-EVAL board and can be easily tailored to any other supported device and development board.

- Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 1) - STMicroelectronics Community

- Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 2) - STMicroelectronics Community

 

I hope this help you.

Thank you.

Kaouthar

 

 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
Aug 22, 2025 3:37 PM UTC

Hello @Rich_P ,

 

Are these resources can help you to start CAN with  Nucleo-L476RG board?

Note that the CAN_Networking  example runs on STM32L476xx devices.

 

If your request is answered,  please click on Accept as Solution on the reply which answered your question.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.