Skip to main content
Olitronik_Lab
Associate
Jul 22, 2025 9:15 AM UTC
Question

STM32CubeIDE 1.19.0 creates "Empty" project from valid .ioc file

I’m using STM32CubeIDE v1.19.0 (Build: 25607_20250703_0907) on Linux, and I’ve run into a recurring issue when creating a project from an existing .ioc file.

When I go to:
File > New > STM32 Project from existing .ioc
and select a valid .ioc file (that opens correctly in STM32CubeMX and works on real hardware), the “Targeted Project Type” field changes automatically from STM32Cube to “Empty”, and the resulting project has no .ioc linked and no code generated.

This issue happens even with:
- Fresh .ioc files
- Clean, empty directories
- New workspaces
- Verified CubeIDE 1.19 installation

However, if I open the same .ioc in **STM32CubeMX (standalone)**, perform a **Save As**, and generate the code with toolchain set to `STM32CubeIDE`, then import the project manually into CubeIDE — everything works fine.

This same issue had occurred in CubeIDE 1.18.x and seems to persist in 1.19.0.

Importantly, this workflow **used to work fine**, and suddenly stopped working **without any visible or intentional change** on my side. It’s as if the IDE stopped recognizing the .ioc structure properly, even though the files are valid.

It appears that the automated project creation wizard fails to recognize valid .ioc files unless they've been freshly saved/generated via CubeMX. Possibly an issue with metadata detection.

Can this be confirmed as a bug? Are there any plans to fix this behavior?

Thanks in advance!

This topic has been closed for replies.

8 replies

Andrew Neil
Super User
Jul 22, 2025 9:18 AM UTC

See the pinned post on this known issue:

STM32CubeIDE STM32Cube project creation issue

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Olitronik_Lab
Associate
Jul 22, 2025 9:40 AM UTC

Thank you for the suggested workaround. I’ve followed all the steps:

  • Disabled auto-refresh in both STM32CubeIDE and STM32CubeMX

  • Deleted the .stmcuFinder folder

  • Restarted STM32CubeIDE

Unfortunately, the issue still persists — the "Targeted Project Type" field remains set to "Empty" when importing a valid .ioc file.

I can continue working by manually generating the project using STM32CubeMX and importing it into CubeIDE, but I hope a permanent fix will be included in a future update.

Thanks again for your support.

Andrew Neil
Super User
Jul 22, 2025 9:51 AM UTC

@Olitronik_Lab wrote:

I hope a permanent fix will be included in a future update.


As the pinned post shows, ST are working on it ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Explorer
Jul 22, 2025 2:02 PM UTC

Same issue here, tried uninstalling and reinstalling the application too. 

Deleted the .meta folder, issue still exist

Created new workspace, issue still exist

Downloaded and installed a fresh installation, issue still exist.

Kindly let me know, if you find a fix for this Bug.

Ghofrane GSOURI
ST Technical Moderator
Jul 22, 2025 2:07 PM UTC

Hello @nit4tin 

Have you followed the instructions mentioned in this post ?

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.