Skip to main content
Sungjae Kim
Associate II
Jan 16, 2025 12:04 PM UTC
Question

Missing dependencies problem (STM32CUBEIDE offline setup)

Hello, I'm having an issue with the STM32CubeIDE configuration.

 

Due to company policy, my development PC does not have internet access, so I need to set up STM32CubeIDE offline.

So, even though I installed the relevant STM32Cube for G0 series, I’m getting a “missing dependencies” error.

Why is it happening? What else do I need to install to resolve this issue?
Also, is there a way to check which dependencies are missing?

 

SungjaeKim_0-1737028701257.png

 

SungjaeKim_1-1737028736800.png
-> I cannot generate code from IOC because some dependencies are missing.
 
SungjaeKim_2-1737028755808.png

 

 Thank you in advance.

 

 
This topic has been closed for replies.

4 replies

ST Technical Moderator
Jan 16, 2025 12:22 PM UTC

Hello @Sungjae Kim ,

To install the package offline, please follow the steps in this article:

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Sungjae Kim
Associate II
Jan 17, 2025 10:39 PM UTC

Hello @Imen.D ,

I followed the instructions from that link, but there wasn’t much progress.

Here are the results I found after further investigation:

  1. If I only download and install version 1.X.0 (without applying any patches), then create a new project using the MCU selector while choosing 1.X.0 as the Cube version, the project is created successfully.

  2. If I apply a patch, the problem persists even when selecting the correct version (in some series the patch applies properly, but usually the issue occurs).

  3. Even with only version 1.X.0 installed, if I create a project through the Board selector, the problem can occur as well (depending on the board).

ST Employee
Jan 20, 2025 8:30 PM UTC

Hi All,

 

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

 

Regards,
Jake

ST Support

Associate
Jun 12, 2025 7:14 AM UTC

i have the same problem i cannot download the patch when my pc is offline is there an update on this?