Skip to main content
JSILV.2
Associate III
Nov 9, 2022 11:00 AM UTC
Question

Issue on Semihosting on CUBE IDE

Salutations for all.

I programmed my CUBE IDE on Debug Mode by the recipe-> https://community.st.com/s/article/how-to-use-semihosting-with-stm32cubeide-and-stm32. It Works.

But when I STOP the running program on CUBE IDE the TARGET STOP the program either. And if I shut off the CUBE IDE, the TARGET seems as not have the Embedded program on it. If I run the TARGET powered alone, it seems like not have any Embedded program.

If I use one program copy but without the semihosting features, using the ST-Link GDB Server, the target works alone even disconnected from CUBE IDE.

Question: What should I do in order to have the Embedded Program into TARGET even Flashing on CUBE IDE by the ST-LINK Open OCD? Is it possible?

The Semihosting Feature is very useful for development.

Regards.

This topic has been closed for replies.

3 replies

Pavel A.
Nov 9, 2022 12:13 PM UTC

A program built with semihosting depends on the debugger and is not expected to run standalone.

(of course, a program can detect that debugger isn't connected, and avoid calling semihosted functions).

JSILV.2
JSILV.2Author
Associate III
Nov 9, 2022 3:16 PM UTC

Dear Pavel.

I am referring that the functions that should runs in the target is OUTSIDE the semihosting ones. For example, I made a simple Blinking LED into the debuggered program with the semihosting and even this LED blinking does not runs. But a clean program (without Semihosting) works as expected even when the Target are standalone.

Comments are welcome.

Regards

Pavel A.
Nov 12, 2022 11:41 PM UTC

So if you want to run standalone, just do not build with semihosting ?

Do you call initialize_monior_handles?