Skip to main content
Efty
Visitor II
May 28, 2023 9:11 PM UTC
Question

How to solve Error Finishing Flash Operation in STM32CubeIDE?

Recurring Error Message in STM32CubeIDE When Running or Debugging a Project. It shows-

'Launching pain Debug' Has encountered a problem.

Error in final launch sequence:

Failed to execute MI command: load

C:\\Users\\USER\\STM32CubelDE\\workspace_1.12.1\\pain\\ Debug\\pain.elf

Error message from debugger back end:

Error finishing flash operation.

and also it showing

"Error in final launch sequence:

Failed to execute MI command:

load C:\\Users\\USER\\STM32CubeIDE\\workspace_1.12.1\\try\\Debug\\try.elf 

Error message from debugger back end:

Error finishing flash operation

Failed to execute MI command:

load C:\\Users\\USER\\STM32CubeIDE\\workspace_1.12.1\\try\\Debug\\try.elf 

Error message from debugger back end:

Error finishing flash operation

Failed to execute MI command:

load C:\\Users\\USER\\STM32CubeIDE\\workspace_1.12.1\\try\\Debug\\try.elf 

Error message from debugger back end:

Error finishing flash operation

Error finishing flash operation"

How to solve this problem? We are using STM32 NUCLEO-F446RE Board

This topic has been closed for replies.

18 replies

AlexanderAustin
Visitor II
Nov 11, 2024 9:06 AM UTC

Hi,

Had a the same issue today and it turns out that I was trying to debug with the project text size that was too big for the micro.

Turned on optimization and it fixed the issue.

Stay Safe!