Skip to main content
Associate II
Apr 22, 2026 3:40 PM UTC
Solved

How to setup debug with STM32N6 in FSBL Load and Run configuration?

How can I debug an STM32N6 project when using a load-and-run configuration? CubeMX generates two separate projects, and I’m able to debug each one individually when the BOOT1 pin is set high. However, it seems that if I only debug the application project, the FSBL never executes, so the system clocks aren’t initialized. What’s the correct approach to debugging both projects together?

I came across a debugging guide, but it only applies to the XIP configuration.

csajiBest answer
Associate II
Apr 23, 2026 3:19 PM UTC

Hi Amel,

 

Thanks for your reply. The article you linked is for the FSBL XiP configuration. Does the same setup apply for FSBL Load and Run configuration?

7 replies

Amel NASRI
ST Technical Moderator
Apr 23, 2026 3:17 PM UTC

Hi @csaji ,

If you are using STM32CubeIDE, this article can be helpful for you: How to debug STM32N6 using STM32CubeIDE.

If you are getting started with STM32N6, several other articles are available on this link.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
csajiAuthorBest answer
Associate II
Apr 23, 2026 3:19 PM UTC

Hi Amel,

 

Thanks for your reply. The article you linked is for the FSBL XiP configuration. Does the same setup apply for FSBL Load and Run configuration?

Associate
May 16, 2026 8:25 AM UTC

Hi csaji,

Did you ever get a solution to this? I'm trying to do exactly the same. I've been through the relevant referenced articles and while there's some good stuff on building for load and run and how to debug XIP, I too want to debug through the FSBL and into the Appli in internal RAM but can't find any info on how to achieve it. Any pointers would be gratefully received.