Skip to main content
Associate III
Jan 19, 2026 8:19 AM UTC
Solved

FreeRTOS Debug Awareness not working

 

Hi everyone,

I am experiencing issues with Task Aware Debugging (FreeRTOS Task List) in the latest version of STM32CubeIDE. The "FreeRTOS Task List" view is either empty or not populating correctly, despite the scheduler running and tasks executing effectively on the hardware.

Environment:

  • IDE: STM32CubeIDE (Latest Version)

  • MCU: STM32H7S3L8H6x

  • FreeRTOS Version: V10.6.2 (CMSIS-RTOS V2 wrapper)

  • STM32Cube 2.0.0

Interestingly enough, the runtimestats itsef are working.

Does anyone have similar issues?

 

Vidar_2-1768810704810.png

 

Vidar_1-1768810683791.png

 

/* USER CODE BEGIN Header */
/*
 * FreeRTOS Kernel V10.6.2
 * Portion Copyright (C) 2017 Amazon.com, Inc. or its affiliates. All Rights Reserved.
 * Portion Copyright (C) 2019 StMicroelectronics, Inc. All Rights Reserved.
 *
 * Permission is hereby granted, free of charge, to any person obtaining a copy of
 * this software and associated documentation files (the "Software"), to deal in
 * the Software without restriction, including without limitation the rights to
 * use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of
 * the Software, and to permit persons to whom the Software is furnished to do so,
 * subject to the following conditions:
 *
 * The above copyright notice and this permission notice shall be included in all
 * copies or substantial portions of the Software.
 *
 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS
 * FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR
 * COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER
 * IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN
 * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE .
 *
 * http://www.FreeRTOS.org
 * http://aws.amazon.com/freertos
 *
 * 1 tab == 4 spaces!
 */
/* USER CODE END Header */
#ifndef __FREERTOS_CONFIG_H
#define __FREERTOS_CONFIG_H

/*-----------------------------------------------------------
 * Application specific definitions.
 *
 * These definitions should be adjusted for your particular hardware and
 * application requirements.
 *
 * These parameters and more are described within the 'configuration' section of the
 * FreeRTOS API documentation available on the FreeRTOS.org web site.
 *
 * See http://www.freertos.org/a00110.html
 *----------------------------------------------------------*/

/* USER CODE BEGIN Includes */
/* Section where include file can be added */
/* USER CODE END Includes */

/* Ensure definitions are only used by the compiler, and not by the assembler. */
#if defined(__ICCARM__) || defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)
#include <stdint.h>
extern uint32_t SystemCoreClock;
/* USER CODE BEGIN 0 */
extern void configureTimerForRunTimeStats(void);
extern unsigned long getRunTimeCounterValue(void);
/* USER CODE END 0 */
#endif
#ifndef CMSIS_device_header
#define CMSIS_device_header "stm32h7rsxx.h"
#endif /* CMSIS_device_header */

#define configENABLE_FPU 1
#define configENABLE_MPU 0

#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 1
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 56 )
#define configUSE_SB_COMPLETED_CALLBACK ( 0 )
#define configUSE_MINI_LIST_ITEM ( 1 )
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)57344)
#define configMAX_TASK_NAME_LEN ( 16 )
#define configGENERATE_RUN_TIME_STATS 1
#define configHEAP_CLEAR_MEMORY_ON_FREE 0
#define configUSE_TRACE_FACILITY 1
#define configUSE_STATS_FORMATTING_FUNCTIONS 1
#define configUSE_16_BIT_TICKS 0
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 16
#define configUSE_RECURSIVE_MUTEXES 1
#define configUSE_APPLICATION_TASK_TAG 1
#define configUSE_COUNTING_SEMAPHORES 1
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 0
#define configRECORD_STACK_HIGH_ADDRESS 0
#define configUSE_POSIX_ERRNO 1
/* USER CODE BEGIN MESSAGE_BUFFER_LENGTH_TYPE */
/* Defaults to size_t for backward compatibility, but can be changed
 if lengths will always be less than the number of bytes in a size_t. */
#define configMESSAGE_BUFFER_LENGTH_TYPE size_t
/* USER CODE END MESSAGE_BUFFER_LENGTH_TYPE */

/* Co-routine definitions. */
#define configUSE_CO_ROUTINES 1
#define configMAX_CO_ROUTINE_PRIORITIES ( 2 )

/* Software timer definitions. */
#define configUSE_TIMERS 1
#define configTIMER_TASK_PRIORITY ( 2 )
#define configTIMER_QUEUE_LENGTH 10
#define configTIMER_TASK_STACK_DEPTH 256

/* The following flag must be enabled only when using newlib */
#define configUSE_NEWLIB_REENTRANT 0

/* CMSIS-RTOS V2 flags */
#define configUSE_OS2_THREAD_SUSPEND_RESUME 1
#define configUSE_OS2_THREAD_ENUMERATE 1
#define configUSE_OS2_EVENTFLAGS_FROM_ISR 1
#define configUSE_OS2_THREAD_FLAGS 1
#define configUSE_OS2_TIMER 1
#define configUSE_OS2_MUTEX 1
#define configTEX_S_C_B_SRAM ( 0x03UL )
#define configTOTAL_MPU_REGIONS 16
/* Set the following definitions to 1 to include the API function, or zero
to exclude the API function. */
#define INCLUDE_vTaskPrioritySet 1
#define INCLUDE_uxTaskPriorityGet 1
#define INCLUDE_vTaskDelete 1
#define INCLUDE_vTaskCleanUpResources 1
#define INCLUDE_vTaskSuspend 1
#define INCLUDE_xTaskDelayUntil 1
#define INCLUDE_vTaskDelay 1
#define INCLUDE_xTaskGetSchedulerState 1
#define INCLUDE_xEventGroupSetBitFromISR 1
#define INCLUDE_xTimerPendFunctionCall 1
#define INCLUDE_xQueueGetMutexHolder 1
#define INCLUDE_xSemaphoreGetMutexHolder 1
#define INCLUDE_pcTaskGetTaskName 1
#define INCLUDE_uxTaskGetStackHighWaterMark 1
#define INCLUDE_uxTaskGetStackHighWaterMark2 1
#define INCLUDE_xTaskGetCurrentTaskHandle 1
#define INCLUDE_eTaskGetState 1
#define INCLUDE_xTaskAbortDelay 1
#define INCLUDE_xTaskGetHandle 1

/*
 * The CMSIS-RTOS V2 FreeRTOS wrapper is dependent on the heap implementation used
 * by the application thus the correct define need to be enabled below
 */
#define USE_FreeRTOS_HEAP_4

/* Cortex-M specific definitions. */
#ifdef __NVIC_PRIO_BITS
 /* __BVIC_PRIO_BITS will be specified when CMSIS is being used. */
 #define configPRIO_BITS __NVIC_PRIO_BITS
#else
 #define configPRIO_BITS 4
#endif

/* The lowest interrupt priority that can be used in a call to a "set priority"
function. */

#define configLIBRARY_LOWEST_INTERRUPT_PRIORITY 15

/* The highest interrupt priority that can be used by any interrupt service
routine that makes calls to interrupt safe FreeRTOS API functions. DO NOT CALL
INTERRUPT SAFE FREERTOS API FUNCTIONS FROM ANY INTERRUPT THAT HAS A HIGHER
PRIORITY THAN THIS! (higher priorities are lower numeric values. */
#define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY 5

/* Interrupt priorities used by the kernel port layer itself. These are generic
to all Cortex-M ports, and do not rely on any particular library functions. */
#define configKERNEL_INTERRUPT_PRIORITY 		( configLIBRARY_LOWEST_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )
/* !!!! configMAX_SYSCALL_INTERRUPT_PRIORITY must not be set to zero !!!!
See http://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html. */
#define configMAX_SYSCALL_INTERRUPT_PRIORITY 	( configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )

/* Normal assert() semantics without relying on the provision of an assert.h
header file. */
/* USER CODE BEGIN 1 */
#define configASSERT( x ) if ((x) == 0) {taskDISABLE_INTERRUPTS(); for( ;; );}
/* USER CODE END 1 */

/* Definitions that map the FreeRTOS port interrupt handlers to their CMSIS
standard names. */
#define vPortSVCHandler SVC_Handler
#define xPortPendSVHandler PendSV_Handler
/* IMPORTANT: After 10.3.1 update, Systick_Handler comes from NVIC (if SYS timebase = systick), otherwise from cmsis_os2.c */

#define USE_CUSTOM_SYSTICK_HANDLER_IMPLEMENTATION 0

/* USER CODE BEGIN 2 */
/* Definitions needed when configGENERATE_RUN_TIME_STATS is on */
#define portCONFIGURE_TIMER_FOR_RUN_TIME_STATS configureTimerForRunTimeStats
#define portGET_RUN_TIME_COUNTER_VALUE getRunTimeCounterValue
/* USER CODE END 2 */

/* USER CODE BEGIN Defines */
/* Section where parameter definitions can be added (for instance, to override default ones in FreeRTOS.h) */
/* USER CODE END Defines */

#endif /* __FREERTOS_CONFIG_H */

Vidar_0-1768810472088.png

 

ST Technical Moderator
Jan 29, 2026 1:41 PM UTC

Hello @Vidar @rnoh 

I launched the Debug Session using FreeRTOS_Mutex example on Nucleo-H7S3L8.

I get the same results on STM32CubeIDE 1.16 and STM32CubeIDE 2.0.

MahmoudBenRomdhane_0-1769693710441.png

STM32CubeIDE 1.16

MahmoudBenRomdhane_1-1769693841105.png

STM32CubeIDE 2.0

MahmoudBenRomdhane_2-1769693991224.png

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

ST Technical Moderator
Jan 23, 2026 7:50 AM UTC

Hello @Vidar 

Let me thank you for posting.

For more investigation, could you please provide your IOC.File.

Thanks

Mahmoud 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
Jan 24, 2026 5:42 PM UTC

Hi,

I encountered a similar issue with STM32CubeIDE (versions 1.19.0 and 2.0.0) while debugging FreeRTOS on Nucléo board (with the V2J46M33 Stlink firmware).

My project had worked last year with 1.16.0. STM32CubeIDE

As a workaround, I used a Jlink SWD probe instead.

Kind regards 

Visitor II
Mar 19, 2026 10:09 AM UTC

Hi all,

I noticed the same behavior as @Vidar had, but after updating to the latest version 2.1.1 on Ubuntu (I don't remember what the exact version was before, but definitely 2.0.0 or higher). Previously everythink worked fine.

After "Suspend", in the Debug View on the left I saw only one thread instead of several. In the console there was also a message "Update threads. Failed collecting threads.". Similar behavior has been observed also here:
- https://community.st.com/t5/stm32cubeide-mcus/freertos-rtos-kernel-awareness-not-working-on-cubeide-1-8-0/td-p/97251
- https://community.st.com/t5/stm32cubeide-mcus/unable-to-use-debugger-while-monitoring-multiple-threads/td-p/764811 

I did a downgrade (full reinstall) to 2.0.0 using Generic Linux sh script, and now it works as previously. 

Platform: Ubuntu 24.04.4 LTS
FreeRTOS version: V10.5.1
MCU: STM32U585 (on custom board)

Best regards,
Tomash