Skip to main content
Associate
Jul 23, 2025 4:22 PM UTC
Question

Could not verify ST device on STM32F407VGT6

I have already updated my CubeIDE to the latest version 1.19.0 available on the official website. After writing the code with it, I attempted to download it to my F407VGT6 via STLink, but the download has never been successful. It always prompts "Could not verify ST device!" When I replaced one board with another, I was able to successfully download. The only difference between the two boards is that the silk-screening of the two VGT6s is slightly different. One has a small circle with "e3" inside and can be downloaded, while the one that cannot be downloaded has "e4" in the circle. I wonder if CubeIDE has not yet adapted to this chip. Has anyone encountered the same situation? I hope to get your solution!

This topic has been closed for replies.

16 replies

Karl Yamashita
Super User
Jul 23, 2025 4:27 PM UTC

Your title suggests that STM32CubeIDE can't be downloaded from ST's site. Maybe change the title to "Could not verify ST device on STM32F407BGT6"

Are you using a development board or a custom board?

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate
Jul 23, 2025 4:32 PM UTC

Thank you. I have already modified the title. Yes, I'm using a custom board.

Andrew Neil
Super User
Jul 23, 2025 4:40 PM UTC

@untitled__666 wrote:

Yes, I'm using a custom board.


Then you need to give details of that board - we can't see it from here!

Please see: How to write your question to maximize your chances to find a solution.

 

Is it, perhaps, a so-called "Black Pill"?

If so, it might have a fake STM32...

 

Also, what ST-Link are you using?

How to recognize a genuine ST-LINK/V2 versus a cloned one.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AScha.3
Super User
Jul 23, 2025 4:28 PM UTC

Try connect with CubeProgrammer, to both, and show, what its telling (chip ID etc.).

If you feel a post has answered your question, please click on " Best Answer ".
Associate
Jul 23, 2025 4:34 PM UTC

untitled__666_0-1753288433185.png

OK, I have uploaded the screenshot of the fault code.

Associate
Jul 23, 2025 4:49 PM UTC

The same board, the same ST-Link programmer, but some chips just can't be programmed. Are the chips fake?!

AScha.3
Super User
Jul 23, 2025 4:57 PM UTC

Maybe...or defective...or write protected (I had this once - no joke ! New chips from mouser - protected !)

So show, pic, not error message - this is useless,  CubeProgrammer, to both, and show, what its telling (chip ID etc.).

so:

AScha3_0-1753289841035.png

 

If you feel a post has answered your question, please click on " Best Answer ".
Associate
Jul 23, 2025 5:05 PM UTC

Where can I find this information in the picture?

TDK
Jul 23, 2025 4:55 PM UTC

Based on the screenshots, seems like the programmer is to blame, probably a fake. Show a picture of your programmer.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."