Skip to main content
Associate II
July 23, 2024
Question

Can we use CAN FD for sending 3000byte of data

Hello,

Our Application need to send 3000 bytes of data over CAN bus

CAN FD allows us to send 64 bytes of data in one frame

Is it feasible to use CAN FD for our application?

Is there any other way, which we can use in CAN?

Also can we use the Multiframe concept in CAN FD?

    This topic has been closed for replies.

    2 replies

    Roger SHIVELY
    ST Employee
    July 24, 2024

    Hello @vividhadhengre 

     

    This post has been escalated to the ST Online Support Team for additional assistance. 

     

    We'll contact you directly.

     

    Regards,

    Roger

    Karl Yamashita
    Principal
    July 24, 2024
    If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source