Skip to main content
Associate II
July 16, 2024
Solved

Is it possible to send 64 bytes of data in the form of Multi frame in CAN FD

 

I am trying to find out whether is it possible to send 64bytes of data in one frame of Multiframe in CAN FD.

i.e First frame will have 64 bytes, Consecutive frame will also have 64 bytes in STM32G0B1KBU6 basically in G0 series MCU

This topic has been closed for replies.
Karl Yamashita
Karl YamashitaBest answer
Principal
July 16, 2024

You have to do it in the FW to send multiple frames. You'll need to use the first byte as a frame indicator. So technically you'll be sending 1 + 63 bytes, where the first byte is frame information and 63 bytes of data.

Create a data structure like this. This is just a reference so you can do it how you like.

 

enum
{
	FIRST_FRAME,
	MORE_FRAMES,
	LAST_FRAME
};

typedef union
{
	struct
	{
		uint8_t data[64];
	}Bytes;
	struct
	{
		unsigned firstFrameActive:2; // 0=firstFrame, 1=moreFrames, 2=lastFrame
		unsigned frameSequenceNumber:6; // 0-63 frames
		uint8_t data[63];
	}Status;
}DataPacket_t;

 

 

Create the canData variable. Populate the data accordingly and just send the packet. This is just a reference showing how the sequence of frames would be sent. I'm not check HAL status here. You'll have to come up with you own packet stuffing using a forloop or whatever method and to be sure a frame has been sent before continuing with the rest of the packets. 

 

		DataPacket_t canData = {0};

		// first packet
		canData.Status.firstFrameActive = FIRST_FRAME;
		canData.Status.frameSequenceNumber = 0;
		canData.Status.data[0] = 0x01; // user will need to fill the rest of the array with data.

		// update pTxHeader to send 64 bytes
		HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &pTxHeader, canData.Bytes.data);

		// next packet
		canData.Status.firstFrameActive = MORE_FRAMES;
		canData.Status.frameSequenceNumber = 1;
		canData.Status.data[0] = 0x01; // user will need to fill the rest of the array with data.

		HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &pTxHeader, canData.Bytes.data);

		// last packet
		canData.Status.firstFrameActive = LAST_FRAME;
		canData.Status.frameSequenceNumber = 2;
		canData.Status.data[0] = 0x01; // user will need to fill the rest of the array with data.

		// update pTxHeader if less than 64 bytes
		HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &pTxHeader, canData.Bytes.data);

 

 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source

6 replies

mƎALLEm
ST Technical Moderator
July 16, 2024

Hello,

Not sure what do you mean by "one frame of Multiframe in CAN FD".

Do you mean you need to send a frame more than 64 bytes and the FDCAN peripheral will split them in 64 byte chunks and send them successively?

If this what you mean, the user needs to do it on his own by software as the FDCAN cell doesn't manage natively this kind of operation. 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate II
July 16, 2024

Hello, Yes actually as per Multiframe concept in CAN 2.0B , we send a first frame with 8 data bytes and wait for FLow control frame(0 byte) and then we send the consecutive frame with data size of 8bytes like this it goes on until the last frame is reached.

In similar way for CAN FD , is it possible to send 64bytes of data in one first frame then wait for Flow Control Frame, then again send the 64bytes of data until the last data frame is reached.

mƎALLEm
ST Technical Moderator
July 17, 2024

Hello @vividhadhengre ,

As stated previously, this is managed by software (application layer: the 7th layer of OSI model) not at the CAN protocol level (link layer). 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.