Skip to main content
Associate III
May 7, 2025 12:53 PM UTC
Solved

Can't use Azure RTOS with H7

Hi,

I am trying to do this tutorial: https://community.st.com/t5/stm32-mcus/how-to-implement-the-usb-device-composite-class-in-stm32-using/ta-p/645017 but I can't find Azure RTOS in Middleware and software Packs. I have already downloaded the packs for azure H7 and placeit here ( C:\Users\XXXXX\STM32Cube\Repository\Packs\STMicroelectronics) but nothing in CudeIDE.
Is enybody have an idea how I can do

Problem_AzureRTOS_1.png

?

Thanks,
G.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
May 9, 2025 2:48 PM UTC

@Gwen1 wrote:

I am using CubeIDE version 1.13.2 and I can't upgrade to an other version because of the firewall.

This is a very old version of CubeIDE. Need to request to your IT team to allow you to do the updates.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

8 replies

TDK
May 7, 2025 12:56 PM UTC

It can be found within the "Software Packs" tab.

TDK_0-1746622570792.png

 

TDK_1-1746622590876.png

 

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Gwen1Author
Associate III
May 7, 2025 12:59 PM UTC

I have only this...

Gwen1_0-1746622702912.png

And I can't open Manage software packs.

TDK
May 7, 2025 1:34 PM UTC

Are you using STM32CubeMX or STM32CubeIDE? And what version? Make sure it's updated.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Gwen1Author
Associate III
May 7, 2025 1:51 PM UTC

I am using CubeIDE version 1.13.2 and I can't upgrade to an other version because of the firewall.

Is my path to the folder is correct ?
In Repository:

Gwen1_0-1746625777618.png

/Packs/STMicroelectronics

Gwen1_1-1746625822394.png

For information I manually create the path.

TDK
May 7, 2025 3:09 PM UTC

I'm not sure manually copying the files is having the same effect as installing them via the program.

I would guess upgrading the version would solve these issues.

"If you feel a post has answered your question, please click ""Accept as Solution""."