Skip to main content
Associate
May 6, 2026 5:50 PM UTC
Question

STLink GDB Server 1.3.0 breaks support on STM32G473CET3

As the title says, the most recent 1.3.0 version of the extension breaks functionality of the debugger for the STM32G473CET3 MCU (and possibly others). By "breaks functionality", I mean that it does not even connect to the MCU anymore.

5 replies

Cartu38 OpenDev
Graduate II
May 6, 2026 8:35 PM UTC
devrim6Author
Associate
May 7, 2026 4:29 AM UTC

Unfortunately it does not :(

The specific error I get is the usual

the system tried to join a drive to a directory on a joined drive

that happens on a variety of problems.

Graduate II
May 7, 2026 5:42 AM UTC

Hi @devrim6,

Is there a more explicit message in the debug console view?

It is possible to add a `"verbose"` attribute set to `true` in the debug configuration to add even more logs to the debug console.

Regards,

Elliot

LaurentL
ST Employee
Jun 17, 2026 12:38 PM UTC

Hello,

Did you succeed to debug your STM32G473 mcu ?

If you haven’t noticed, some extensions have been fixed and might solve your issue.

See the post :

 

Regards,

Laurent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.