Skip to main content
Adam Hamilton
Senior
Oct 20, 2025 11:00 PM UTC
Question

Include Device Specific Header Files

For quite some time now, both with the STM32CubeIDE and now with this VSCode extension, empty projects lack the device specific header files that will be needed to work with the selected device. Usually, the way I have done it in the past is that I navigate to the STM32Cube repository folder to copy about six header files and the system source file to my project directory. It is cumbersome.

I believe I have made a post regarding this before back in 2020, Why does creating an empty project not add header files 

Some workarounds were to create a Cube project and then delete the .ioc and HAL files as well as removing the compiler defined symbols that specify to use the HAL driver. This works and I have been using this method. However, it is a bit cumbersome, and I think that if the empty project already contain bare-bones files for the selected device, it should also include the necessary device specific files as well to save some of the burden of locating the relevant files and copying them across

Thanks

This topic has been closed for replies.

2 replies

ST Employee
Oct 21, 2025 5:45 AM UTC

@Adam Hamilton, thank you for sharing your feedback again. We truly appreciate and welcome input that helps us prioritize our roadmap.

Please see https://community.st.com/t5/stm32cubeide-for-visual-studio/quot-create-empty-project-quot-does-not-provide-cmsis-files/td-p/819374 and feel free to add your comments.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Adam Hamilton
Senior
Nov 4, 2025 7:36 AM UTC

Hi @vincent_grenet I have given some feedback on the other thread that you linked. I would like to know where it is at because the accepted solution on that thread doesn't make a lot of sense.

I don't want this to go by the wayside because I think that providing a minimal working project should be the goal.