Skip to main content
Associate II
Jun 10, 2026 9:43 AM UTC
Solved

How to select a specific STLInk for debugging in VSCode

I have multiple STLinks on multiple Nucleo boards.  I can debug only if I connect one at a time, but it is tedious to connect and reconnect to switch boards. When I plug in multiple devices I see them listed (bottom left) but I can’t work out how to select a specific STLink to use.  If I try to debug it fails with a “bound doStepConnectToTarget Failed: could not connect: Operation timed out.” and suggests I open launch.json.

Disconnecting the cables is additionally tedious because I’m using the VCP on each, and disconnecting breaks the connection to the terminals, which then all need to be reconnected.

I know that with the stand-alone STM32CubeIDE it possible to have separate configurations for each STLink (defined by Serial ID) and then I select the one to use as needed, without having to disconnect any hardware (and the VCPs for the devices I’m not debugging stay connected).

Is there a way to specify the STLink serial ID to use in the launch.json file?  In VSCode I notice there is a button to copy the Serial ID to the clipboard - but how do I use that?

There’s a Knowledge base article here  by ​@Nawres GHARBI  but there is no mention of the STLink Serial ID. Maybe there is another way to do this?

I’m using this launch configuration that was auto generated:

    "configurations": [
{
"type": "stlinkgdbtarget",
"request": "launch",
"name": "STM32Cube: Launch ST-Link GDB Server",
"origin": "snippet",
"cwd": "${workspaceFolder}",
"preBuild": "${command:st-stm32-ide-debug-launch.build}",
"runEntry": "main",
"imagesAndSymbols": [
{
"imageFileName": "${command:st-stm32-ide-debug-launch.get-projects-binary-from-context1}"
}
]
}
]


I’m on macOS, and using two NUCLEO-F303K boards and two NUCLEO-H7S3L8 boards. VSCode 1.123.1 and STM32CubeIDE for VSCode v3.9.0

Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
Jun 10, 2026 12:39 PM UTC

Hi ​@SJB 

The only way is to use the Serial ID. 

As you said before, copy it using the copy ID button then add this parameter in the launch file 
"serverSerialNumber": "Copied_Serial_ID_from_button",              

4 replies

Andrew Neil
Super User
Jun 10, 2026 9:57 AM UTC

with the stand-alone STM32CubeIDE it possible to have separate configurations for each STLink (defined by Serial ID) 

 

Indeed it is - and that is an invaluable feature!

I don’t use VSCode yet, but not being able to do this would be a major blocking issue for me!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
Jun 10, 2026 12:39 PM UTC

Hi ​@SJB 

The only way is to use the Serial ID. 

As you said before, copy it using the copy ID button then add this parameter in the launch file 
"serverSerialNumber": "Copied_Serial_ID_from_button",              

SJBAuthor
Associate II
Jun 10, 2026 1:08 PM UTC

​@Nawres GHARBI  Thank you. That now works for me. I now have two separate configuration in launch.json that I can select from the drop-down box in the Debug tab.

BTW, I would never have guessed that that setting name. I did try ‘serialID’ as that's what it’s called when it’s copied.  Also tried targetID and serialNumber based on some googling.   Maybe it's obvious when you know.

Could I suggest an update of your useful Knowledge base article, as I’m sure its not an unusual to have multiple ST-Links connected.

Nawres GHARBI
ST Technical Moderator
Jun 10, 2026 2:30 PM UTC

STM32CubeIDE for VS Code debug configuration (launch.json) | Community

 

but I didn’t describe all the parameters. You can type in the launch.json “server” and in the help popup will show you all the parameters related to your debugger with a little description