Skip to main content
Associate
Oct 19, 2025 12:05 AM UTC
Solved

Bad CMake Executable and Missing Board from project setup.

Trying to get the STM32CubeIDE for VSCode working on MacOS. I am on the latest version I think it is 3.6.4.
I installed the extension according to instructions and I made a project for my NUCLEO-446RE with CubeMx.

When I open the folder in VSCode it throws a Bad CMake Executable Error when I open the Setup STM32Cube project(s) section. In the search box in this section it also seems the NUCLEO-446RE is missing as well.

I am not sure what is going on I tried uninstalling everything and reinstalling. I do have it in its own profile the only extensions in there are copilot and the STM32 Bundle in its entirety.

Another note: I do not have a local cmake installed so there should be no conflict there.

Any help would be appreciated.

This topic has been closed for replies.
Julien D
Julien DBest answer
ST Employee
Oct 20, 2025 11:58 AM UTC

Hello,

As stated on another post (https://community.st.com/t5/stm32cubeide-for-visual-studio/quot-an-error-occurred-while-synchronizing-metadata-quot-on-vs/m-p/848848#M1268) the issue had been analyzed, and a fix is about to be deployed.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

9 replies

wljrAuthor
Associate
Oct 19, 2025 2:45 AM UTC

There are also errors being thrown while trying to sync the packs. When I ran core pack sync in the integrated terminal the more descriptive error is Error during metadata sync: Error: Unexpected close tag. 

This maybe why the Nucleo board does not show up.

ST Employee
Oct 19, 2025 9:25 PM UTC

@wljr, I can confirm that if there is a pack sync issue, none of the STM32 portfolio devices can be promoted to you.

Are you experiencing this kind of issue? Please see this link for reference:
https://community.st.com/t5/stm32cubeide-for-visual-studio/cube-pack-sync-error-via-vscode-proxy/td-p/847146

Please try executing the following command in the VSCode integrated terminal:

cube pack sync

Let's share back please the result (log trace & notification details)

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
wljrAuthor
Associate
Oct 19, 2025 10:56 PM UTC

@vincent_grenet 

CMake issue is resolved by installing a copy locally like you suggested. Now the only issue is the pack list.

As far as I am aware I am not running any proxy's but this is the result of my cube pack sync and the error in the notification area when it tries to synch the pack list.

Screenshot 2025-10-19 at 6.46.54 PM.png

ST Employee
Oct 19, 2025 9:38 PM UTC

@wljr, regarding the CMake issue, if you do not have CMake installed locally, it is fully supported and expected to face an error. Let me explain what happens behind the scenes.

The STM32CubeIDE for Visual Studio Code extension pack relies on the widely used Microsoft CMake Tools extension. This extension attempts to perform a CMake configure step on any CMakeLists.txt file added to the VSCode workspace. If CMake is not available on your host, it will fail. This is outside of STMicroelectronics’ control since the extension is not ours.

Our responsibility is to notify you when a CMake project is detected, asking if you want to apply STM32Cube’s extra features. If you confirm, STM32Cube will set up the proper tools, including CMake. After setup completes, STM32Cube will trigger a CMake configure process, which should succeed.

vincent_grenet_0-1760909745580.png

Just in case the notification is missing, let's manually invoke the process by using the following setup action:

vincent_grenet_1-1760909804366.png

 



 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Julien D
Julien DBest answer
ST Employee
Oct 20, 2025 11:58 AM UTC

Hello,

As stated on another post (https://community.st.com/t5/stm32cubeide-for-visual-studio/quot-an-error-occurred-while-synchronizing-metadata-quot-on-vs/m-p/848848#M1268) the issue had been analyzed, and a fix is about to be deployed.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.