Skip to main content
This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
November 24, 2020

Hi @MVENN.1​ ,

Only the last version 2.6 is supported on Ubuntu 20.04.

And since this version the JRE is bundle inside STM32CubeProgrammer and no longer need extra JRE package.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

43 replies

MVENN.1
MVENN.1Author
Associate III
November 26, 2020

HI,

I'm using USB -C power supply ( 5.1 V /3A )Raspberry Pi

Here they given l given like https://community.st.com/s/question/0D50X0000Bftr1ySQA/power-supply-for-stm32mp157cdk2

And also I'm added -tm 20000

still problem is there

please give suggestion

moveon@moveon-VirtualBox:~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.6.0          

   -------------------------------------------------------------------

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

SN     : 0034001A3438510438333630

FW version : 0x0110

Device ID  : 0x0500

Device name : STM32MP1

Device type : MPU

Device CPU : Cortex-A7

Start Embedded Flashing service

Error: The file FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv does not exist, please check the file's path

Error: TSV flashing service failed

moveon@moveon-VirtualBox:~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package$ ls

en.FLASH-stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12.tar.xz stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12

moveon@moveon-VirtualBox:~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package$ cd stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/images/stm32mp1/

arm-trusted-firmware/    flashlayout_st-image-weston/ scripts/           

bootloader/         optee/            

moveon@moveon-VirtualBox:~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package$ cd stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/images/stm32mp1/

moveon@moveon-VirtualBox:~/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/images/stm32mp1$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.6.0          

   -------------------------------------------------------------------

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

SN     : 0034001A3438510438333630

FW version : 0x0110

Device ID  : 0x0500

Device name : STM32MP1

Device type : MPU

Device CPU : Cortex-A7

Start Embedded Flashing service

Memory Programming ...

Opening and parsing file: tf-a-stm32mp157c-dk2-serialboot.stm32

 File     : tf-a-stm32mp157c-dk2-serialboot.stm32

 Size     : 237896 Bytes

 Partition ID : 0x01 

Download in Progress:

[==================================================] 100% 

File download complete

Time elapsed during download operation: 00:00:00.640

RUNNING Program ... 

 PartID:   :0x01 

Start operation done successfully at partition 0x01

Flashlayout Programming ...

[==================================================] 100% 

Running Flashlayout Partition ...

Flashlayout partition started successfully

Memory Programming ...

Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32

 File     : u-boot-stm32mp157c-dk2-trusted.stm32

 Size     : 904820 Bytes

 Partition ID : 0x03 

Download in Progress:

[==================================================] 100% 

File download complete

Time elapsed during download operation: 00:00:01.566

RUNNING Program ... 

 PartID:   :0x03 

reconnecting the device ...

Error: 

Unable to reconnect the target device: time out expired

Error: Start operation failed at partition 0x03

Error: TSV flashing service failed

Thanks.

PatrickF
ST Employee
November 26, 2020

Hi @MVENN.1​ 

that's sound very like a VM configuration issue, it is described in the FAQ link we already provided to you (https://community.st.com/s/article/FAQ-STM32MP1-STM32CubeProgrammer-USB-reconnect-error-at-STM32MP1-boot-device-flashing).

Abstact:"

  • If you are using a VM, check the USB 'connection' between Linux and Windows as uBoot reconnect using a different USB identification and might not be 'routed' to the VM.
  • In VMWare, you have a menu Player/Removable Devices where you can choose which devices that belong to Virtual Machine or to Windows. In VirtualBox it should have similar setting.
  •  

When uBoot start up, check at that time in your VM if you have 'USB download gadget@Device ID /0x500, @Revision ID /0x0000)' as a new removable device to 'connect' to your Virtual Machine.

"

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
MVENN.1
MVENN.1Author
Associate III
November 26, 2020

Hi PatrickF ( ST Employee )

Thanks for your reply.

Its working everything really thanks for your support.

after adding VM in 'USB download gadget@Device ID /0x500, @Revision ID /0x0000)'  and select in VM.

like

Thanks.