Skip to main content
mishuk
Associate III
September 3, 2023
Question

STM32MP1 pixel format RGB666

Hello,

according to drivers/gpu/drm/stm/ltdc.c stm hardware supports these pixel formats:

enum ltdc_pix_fmt {
PF_NONE,
/* RGB formats */
PF_ARGB8888, /* ARGB [32 bits] */
PF_RGBA8888, /* RGBA [32 bits] */
PF_RGB888, /* RGB [24 bits] */
PF_RGB565, /* RGB [16 bits] */
PF_ARGB1555, /* ARGB A:1 bit RGB:15 bits [16 bits] */
PF_ARGB4444, /* ARGB A:4 bits R/G/B: 4 bits each [16 bits] */
/* Indexed formats */
PF_L8, /* Indexed 8 bits [8 bits] */
PF_AL44, /* Alpha:4 bits + indexed 4 bits [8 bits] */
PF_AL88 /* Alpha:8 bits + indexed 8 bits [16 bits] */
};

which corresponds to list of pixel format that I get from modetest -M stm | grep format:

formats: AR24 XR24 RG24 RG16 AR15 XR15 AR12 XR12 C8

My question is : does STM hardware support RGB666 pixel format ?  If yes, how should I patch stm driver to handle this pixel format ?

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
September 4, 2023
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
mishuk
mishukAuthor
Associate III
September 5, 2023

No, these posts won`t help.  I asked not about Device Tree Configuration, but about RGB control inside hardware and corresponding driver. Current STM driver implementation (drivers/gpu/drm/stm/ltdc.c) lacks pixel format RGB666.  I ask, how can I add this pixel format, if it is supported by STM hardware. If it is not supported, I suppose, it makes no sense for adding pixel format inside driver.