Skip to main content
MWoło.2
Senior III
October 23, 2021
Question

ksz8041 bring up

It seems that I have a problem with DMA, but I'm not sure. Would you please take a look at the below screen

0693W00000FDX7aQAH.pngDts looks

0693W00000FDX7zQAH.jpg0693W00000FDX84QAH.jpgI intend to achieve MII with self-generated quartz.

Unfortunately, I'm stuck on this "Failed to reset the DMA".

This topic has been closed for replies.

22 replies

MWoło.2
MWoło.2Author
Senior III
November 15, 2021

I measured both RXC and TXC using an oscilloscope, and is no sine waveform on both what I do wrong.

PatrickF
ST Employee
November 16, 2021

Hi,

both RXC and TXC come from PHY. So, some investigations are needed around PHY:

From SW log, I understand KSZ8041 is discovered, so the MDIO bus is working. Maybe also linked to a microchip driver issue in MII mode.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent