Get ready for the STM32 Summit 2026 | Online, November 3
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Most recent activity
Hello, I am able to compile the M4 examples and it looks as though they run as expected ( I can see the log trace on the A7 side from the linux console). I would like to examine the log trace from the M4 side also as I would like to modify some of these examples for further use. In the OpenAMP_TTY_echo example (main.c) are the following lines log_info("Cortex-M4 boot successful with STM32Cube FW version: v%ld.%ld.%ld \r\n", ((HAL_GetHalVersion() >> 24) & 0x000000FF), &nb
How to install mono on my STM32MP157C-DK2?Thanks
I guess most have noticed the recent anouncement of the STM32MP1, a dual core unit with a Cortex A7 and a M4.Hard data seem a bit scarce yet, though.What toolchain will support this combo, and when ?Does the mentioned STLink V3 support concurrent debugging of both cores ?What about an evaluation hardware ?And a Linux version ?And what about the interest in dual-cores on customer's side, or is it just a case of # metoo ? ;)
Are there any resources that show how to configure the communication peripherals ( USB,. USART) when using the STM32MP1 based parts. I tried to configure a USART and USB peripheral, but STMCube generates a dialog that indicates that this peripheral must be configured by hand. I checked in the examples under STM32CubeMP1 repo and in the UART exampless, it looks like the UART pins are not configured ( looks like MX_GPIO_Init just enables the clocks ). I would like to use the USART and USB peripherals from the M4 side on this processor
Hello, all!For some time now I have been trying to come up with a solution to connect 2 cameras of 480X640 resolution and several peripherals to a low-power MCU. I keep hitting a wall, because it seems that this endeavor is not suitable for an MCU - the large RAM required to host 600K image, the fact that I can't connect 2 USB / DCMI cameras and need several MCUs that defeat the purpose, the fact that having a DCMI, an FSC and several peripherals on the same MCU, that is also, low-power, is unheard of..So, I'm trying my luck with an MPU:does ST offer a low-power MPU that has a large RAM, >100 IOs, and most importantly - can interface 2 USB cameras?Is there a tool like MCU FInder for MPUs?Are there guides for getting strated with ST MPUs?Is it possible to perform an Over The Air Update with an ST MPU?Thanks!** Partial answers will be much appreciated as well. Just starting off with the MPU direction, and want to understand if it suits my needs and how challenging it would be.
Hello, I'm trying to evaluate the STM32MP1 using a STM32MP157C-DK2. I followed this getting started guide and successfully flashed the board, even though the archive downloaded has a slightly different name than mentioned in the guide. I set the boot switches to the on position and reset the board, which is showing the UBoot splash screen. But afterwards it goes dark, no Linux splash screen, Weston desktop or GTK demo launcher to be seen anywhere. The system itselfs seems to work correctly, as pressing the reset button with minicom connect shows (see log attached).The big LED next to the ST-LINK is constantly red. A small LED close by flashes two times blue, then pauses, followed by another two flashes...What am I missing here? Shouldn't the board boot to the GTK demo launcher automatically? Best Regards,Matt
..
Hi everybody!I working on a simple project but with some sensors and co.I'm newbie with the STM32 and I want to try to port the project from the ATmega2560 to the STM32.But witch chip? I need :> SPI for an TFT screen 2.2" (ILI9340C or ILI9341)> SPI for a MicroSD Card> BMP180 sensor> 2 pins interup> 3 indepedants Pins PWM> 2 ADC> RTC time> One Serial for bluetooth HC-05> One Serial for an GPS L80> One Serial for connect an external probe> 10 digital Input> 4 digital Output> min 72Mhz for the sreen> All pin in 3.3vQuestion :> Minimum 64K of program space ?> Flashing the MPU directly with the USB port ?> Possible to program all from the Arduino IDE ? ( with the right card )Thanks! =)
For an application we are investigating this processor and have two questions,We want to connect an external chip to the FMC bus. It is somespecialized ASIC handling some real-time communication.I don't see the option in the STM32Cube to active the FMC in SRAM mode?But I see it in the reference manual. Is it available?Is the SRAM also accessible by the Cortex M4? What I understand from the refence manual is that it is supported.
Hi,I have succesfully built a image st-example-image-qt from the DISTRO openstlinux-eglfs.I have deployed the image on sd card, and played it on STM32MP157C-DK2.System is booting without a problem, and the splashscreen was shown.Then, I tried one of Qt examples e.g.:root@stm32mp1:~# /usr/share/examples/opengl/hellowindow/hellowindowqt.qpa.input: X-less xkbcommon not available, not performing key mappingCould not set DRM mode for screen DSI1 (Permission denied)Could not queue DRM page flip on screen DSI1 (Permission denied)Could not queue DRM page flip on screen DSI1 (Permission denied)Could not queue DRM page flip on screen DSI1 (Permission denied)...export QT_QPA_EGLFS_ALWAYS_SET_MODE="1"export QT_QPA_EGLFS_INTEGRATION="eglfs_kms"does not help!What can be the Issue here?
HiI got an STM32MP157C-DK2 during the Embedded World.But Windows7 isn't detecting the DFU ... It detects only the STLink (UART) ....Same issue in a Ubuntu-16 (which is running in VirtualBox on the same Windows 7)Any suggestion?Regards Francesco
Hi,I'm planning to buy an STM32MP1 discovery kit (when available) and I'm wondering how to get access to the distribution package. I read on wiki.st.com that I have to request these rights to my ST support contact but I can't found out how to do it.Thanks in advance
I downloaded Yocto_SDK Software Version- 1.0.0 for STM32MP151C. The environment setup file name is - "environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi". Does it mean that this SDK is tailored for Wayland implementation? We intend to use raw framebuffer device. As of now we have no plans of using X11 or Wayland. Can we use this SDK?
Hello,until now, all STM32 datasheets do not specify JTAG/SWD interface characteristics except for STM32H7: 6.3.33 JTAG/SWD interface characteristics.The JTAG/SWD interface characteristics should be specified.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.