Skip to main content
BryanWang
Associate II
December 5, 2019
Solved

Failed to boot the kernel via TFTP from U-Boot on STM32MP157c DK2 board.

Hello, I am trying to boot kernel via TFTP from U-Boot on my DK2 board, after retrieving PXE configuration file successfully, the uImage failed to retrieved. However, I could successfully get uImage file by u-boot tftp command.

​

The steps I am following is https://wiki.st.com/stm32mpu/wiki/How_to_boot_the_kernel_via_TFTP_from_U-Boot#pxelinux.cfg_directory.

​

I have installed tftp servers on my Ubuntu, and the pxelinux.cfg directory, PXE configuration file, uImage, stm32mp157c​-dk2.dtb are all under tftp directory.​

​

/tftpboot
 
 |---- mmc0_stm32mp157c-dk2.extlinux
 
 | |--------- ​pxelinux.cfg
 
 | |------------ 01-00-80-e1-42-51-72
 
 | |--------- uImage
 
 | |--------- stm32mp157c-dk2.dtb

​

my PXE configuration file is:

menu title Select the boot mode
DEFAULT sdcard
LABEL sdcard
	KERNEL uImage
	FDT stm32mp157c-dk2.dtb
	APPEND root=/dev/mmcblk0p6 rootwait rw earlyprintk console=ttySTM0,115200

The TF-A, u-boot, uImage, dtb file are all released by ST.

​

​The following is the u-boot log:

STM32MP> env print ipaddr
ipaddr=192.168.1.102
STM32MP> env print ethaddr
ethaddr=00:80:e1:42:51:72
STM32MP> env print serverip
serverip=192.168.1.101
STM32MP> env print netmask
netmask=255.255.255.0
STM32MP> run bootcmd_pxe
BOOTP broadcast 1
DHCP client bound to address 192.168.1.102 (2 ms)
missing environment variable: pxeuuid
Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/pxelinux.cfg/01-00-80-e1-42-51-72
Using ethernet@5800a000 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.102
Filename '/mmc0_stm32mp157c-dk2_extlinux/pxelinux.cfg/01-00-80-e1-42-51-72'.
Load address: 0xc4200000
Loading: #
 87.9 KiB/s
done
Bytes transferred = 181 (b5 hex)
Config file found
Select the boot mode
1: sdcard
Enter choice: 1
1: sdcard
Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/uImage
Using ethernet@5800a000 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.102
'.lename '/mmc0_stm32mp157c-dk2_extlinux/uImage
Load address: 0xc2000000
Loading: *
TFTP error: 'File not found' (1)
Not retrying...
 for failure retrieving kernel
STM32MP> tftp mmc0_stm32mp157c-dk2_extlinux/uImage
Using ethernet@5800a000 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.102
Filename 'mmc0_stm32mp157c-dk2_extlinux/uImage'.
Load address: 0xc2000000
Loading: #################################################################
 #################################################################
 #################################################################
 #################################################################
 #################################################################
 #################################################################
 ################################################################
 1.9 MiB/s
done
Bytes transferred = 6652480 (658240 hex)
STM32MP>

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
December 5, 2019

Hi @BryanWang​ 

Did you see this existing post :

https://community.st.com/s/question/0D50X0000BJ0vxhSQB/failed-boot-via-tftp

May it help to give solution or hints ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
December 5, 2019

Hi @BryanWang​ 

Did you see this existing post :

https://community.st.com/s/question/0D50X0000BJ0vxhSQB/failed-boot-via-tftp

May it help to give solution or hints ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
BryanWang
BryanWangAuthor
Associate II
December 6, 2019

Hi Olivier,

yes, this post works. Thanks.