Skip to main content
Jzhua
Associate III
September 9, 2019
Solved

failed boot via tftp

I tried booting via TFTP boot and got the following reply

​

BOOTP broadcast 1

BOOTP broadcast 2

BOOTP broadcast 3

DHCP client bound to address 192.168.1.2 (766 ms)

missing environment variable: pxeuuid

missing environment variable: bootfile

Retrieving file: pxelinux.cfg/01-00-80-e1-42-56-51

Using ethernet@5800a000 device

TFTP from server 192.168.1.94; our IP address is 192.168.1.2

Filename 'pxelinux.cfg/01-00-80-e1-42-56-51'.

Load address: 0xc4200000

Loading: #

     0 Bytes/s

done

Bytes transferred = 248 (f8 hex)

Config file found

Select the boot mode

1:   Linux 4.19.9

Enter choice: 1:    Linux 4.19.9

missing environment variable: bootfile

Retrieving file: uImage

Using ethernet@5800a000 device

TFTP from server 192.168.1.94; our IP address is 192.168.1.2

'.lename 'uImage

Load address: 0xc2000000

Loading: *

TFTP error: 'File not found' (1)

Not retrying...

 for failure retrieving kernel​

​

this is my /tftpboot tree

​

.

├── pxelinux.cfg

│  ├── 01-00-80-e1-42-56-51 -> default-arm-stm32mp

│  └── default-arm-stm32mp

├── stm32mp157c-dk2.dtb

└── uImage

​

I tested the TFTP server is available, all files are available for download.

​

Where is the problem?

This topic has been closed for replies.
Jzhua
JzhuaBest answer
Associate III
September 10, 2019

The reason is default-arm-stm32mp file use CRLF not LF,now it work

4 replies

Olivier GALLIEN
ST Technical Moderator
September 9, 2019

Hi @Jzhua​ 

Can you please confirm you have followed this guideline

https://wiki.st.com/stm32mpu/wiki/How_to_boot_the_kernel_via_TFTP_from_U-Boot

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Jzhua
JzhuaAuthor
Associate III
September 9, 2019

yes,I was followed this guideline​

Olivier GALLIEN
ST Technical Moderator
September 9, 2019

Hi @Jzhua​ 

I succeed to boot on tftp with the procedure.

content of my tftpboot directory ( I used artifact from defaut st-image-weston stm32mp1-disco image)

/tftboot :

drwxrwxr-x 2 osboxes osboxes  4096 Sep 9 12:44 pxelinux.cfg

-rwxrwxrwx 1 osboxes osboxes  69510 Sep 9 10:31 stm32mp157c-dk2--4.19-r0-stm32mp1-disco-20190909122915.dtb

lrwxrwxrwx 1 osboxes osboxes   68 Sep 9 12:31 stm32mp157c-dk2.dtb -> /tftpboot/stm32mp157c-dk2--4.19-r0-stm32mp1-disco-20190909122915.dtb

lrwxrwxrwx 1 osboxes osboxes   59 Sep 9 12:30 uImage -> /tftpboot/uImage--4.19-r0-stm32mp1-disco-20190909122915.bin

-rwxrw-rw- 1 osboxes osboxes 6555552 Sep 9 10:29 uImage--4.19-r0-stm32mp1-disco-20190909122915.bin

Content of pxelinux.cfg/01-00-80-e1-42-4c-e8

menu title Select the boot mode

DEFAULT ramfs

LABEL ramfs

KERNEL uImage

FDT stm32mp157c-dk2.dtb

APPEND rootwait rw earlyprintk console=ttyS3,115200

I need to remove line 'INITRD uInitrd' in order it works.

Problem looks to come from this broken line in your trace :

TFTP from server 192.168.1.94; our IP address is 192.168.1.2

'.lename 'uImage

On my side I got :

TFTP from server 10.xx.***.49; our IP address is 10.xx.***.120          

Filename 'uImage'.

Check for any syntax issue ?

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Jzhua
JzhuaAuthorBest answer
Associate III
September 10, 2019

The reason is default-arm-stm32mp file use CRLF not LF,now it work