Skip to main content
BG.3
Associate III
April 9, 2022
Question

DDR Bus Test Error in STM32MP157AAD3 before FSBL, How to resolve this?

Our board is similar to STM32MP157C-DK2 Disco board - All the Developer packages have been installed, When the power supply is given, all the test point voltages are in desired level. But the MPU not even clearing FSBL and exit with

ERROR: DDR addr bus test: can't access memory @ 0xc0000004

PANIC at PC : 0x2ffdf9d9

Exception mode=0x00000016 at: 0x2ffda000

What is the issue and how we can address?

This topic has been closed for replies.

10 replies

PatrickF
ST Employee
April 11, 2022

Hi,

There is many FAQ which could help:

from this page : https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure you could find many links/information.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
BG.3
BG.3Author
Associate III
April 11, 2022

Thank you so much for responding. I'll look into it.

DG_it
Associate
March 20, 2023

Hello, have you solved the problem? I have encountered a similar problem.

PatrickF
ST Employee
September 5, 2024

Hi,

error message is usually just not enough to help.

We need more information on your setup (HW, SW, board, etc...) and the check you already done (supplies, soldering, etc...).
For DDR, even if slightly outdated, this page could help to go further

https://community.st.com/t5/stm32-mpus/faq-stm32mp1-how-to-validate-the-stm32mp1-dram-connection-on-pcb/ta-p/49270

Community is not a simple question/answer tool, but a sharing platform intended to raise knowledge and allows people to find themself the solution or the path for deeper investigation.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
asadullah4571
Associate III
September 6, 2024

I think the ISSUE with the PMIC it won't supply the voltage to the ddr.
I Read the datasheet of PMIC i Found that my DDR is connected to PMIC buck 2 which is RANK 0.
i do not know anything of that. 
who are RANK 0 in PMIC are not supplied the power.
so where i need to modify and TF-A then it work.

PatrickF
ST Employee
September 6, 2024

Hi,

It is normal to have DDR supplies as RANK0 (not powered by default).

The DDR supplies are started in right sequence by the TF-A SW. There is no need to modify SW, but maybe you have issue on your Device Tree regarding DDR related supplies definitions.

If your HW around STPMIC1 and DDR3L is same than STM32MP157D-DK2, please look to the related TF-A DT which could help you to align your own DT: https://github.com/STMicroelectronics/arm-trusted-firmware/blob/v2.8-stm32mp/fdts/stm32mp15xx-dkx.dtsi (some other DT files might be involved as well)

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent