Skip to main content
darla14
Associate III
Feb 11, 2022 5:07 AM UTC
Question

Creating a flashable backup of sd card image

Hello,

I have sd card with lots of things configured.To save time I want to create backup of this card which I can flash later.

Is there any official way to take the backup of the STM32MPU sd card image and also a way to flash the same image on new SD card (with the starter package already installed as well as a new card from the factory ).

Looking for an STM32MPU DK2 F board but I think must be valid for all boards

Regards,

Thanks in Advance !

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
Feb 11, 2022 7:49 AM UTC

Hi @darla14​ ,

See this community post already addressing same question :

https://community.st.com/s/question/0D53W00000qwKLQSA2/how-to-backup-partitions-from-sd-card-image-and-to-flash-it-later

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Olivier GALLIEN
ST Technical Moderator
Feb 11, 2022 7:51 AM UTC
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.