Question
Installing the x-linux-ai Tool
I tried installing x-linux-ai by following the instructions in the [X-LINUX-AI Starter package] .
but I was unable to install it due to an error.
root@192-168-1-59:~# apt-get update
The software package is provided AS IS, and by downloading it, you agree to be
bound to the terms of the software license agreement (SLA).
The detailed content licenses can be found at
https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses.
https://www.st.com/resource/en/additional_license_terms/additional-license-terms-for-x-linux-isp.html
Hit:1 http://packages.openstlinux.st.com/6.2.1 scarthgap InRelease
Hit:2 http://extra.packages.openstlinux.st.com/ISP/6.2.1 scarthgap InRelease
Reading package lists... Done
root@192-168-1-59:~# apt-get install x-linux-ai-tool
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
E: Unable to locate package x-linux-ai-tool
root@192-168-1-59:~# apt-get install x-linux-ai-tool
My setup consists of a custom board based on the STM32MP255F, onto which I ported Linux from ecosystem 6.2.1.
root@192-168-1-59:/etc# cat /etc/os-release
ID=openstlinux-weston
NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro)"
VERSION="5.0.17-snapshot-20261106 (scarthgap)"
VERSION_ID=5.0.17-snapshot-20261106
VERSION_CODENAME="scarthgap"
PRETTY_NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 5.0.17-snapshot-20261106 (scarthgap)"
CPE_NAME="cpe:/o:openembedded:openstlinux-weston:5.0.17-snapshot-20261106"
root@192-168-1-59:/etc# uname -r
6.6.129-ga61679df7e09-dirty
Does x-linux-ai not support ecosystem 6.2.1?
I also cannot install 3D Cube Extra using the Python GTK launcher.
I had no issues when using ecosystem 6.0.0, which I had ported for the same board.