Skip to main content
Associate II
Nov 26, 2025 3:03 AM UTC
Solved

Unable to include X-CUBE-MEMS1 in I2C example project

I am encountering a build failure in the I2C_OneBoard_Communication_PollingAndIT_Init project after integrating the X-CUBE-MEMS1 software expansion pack.

 

D:/STM32Cube/I2C_OneBoard_Communication_PollingAndIT_Init/Drivers/STM32WBAxx_HAL_Driver/Src/stm32wbaxx_hal_dma.c:185:10: fatal error: stm32wbaxx_hal.h: No such file or directory
 185 | #include "stm32wbaxx_hal.h"
 | ^~~~~~~~~~~~~~~~~~
compilation terminated.
D:/STM32Cube/I2C_OneBoard_Communication_PollingAndIT_Init/Drivers/STM32WBAxx_HAL_Driver/Src/stm32wbaxx_hal_dma_ex.c:478:10: fatal error: stm32wbaxx_hal.h: No such file or directory
 478 | #include "stm32wbaxx_hal.h"
 | ^~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [Drivers/STM32WBAxx_HAL_Driver/subdir.mk:46: Drivers/STM32WBAxx_HAL_Driver/stm32wbaxx_hal_dma.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Drivers/STM32WBAxx_HAL_Driver/subdir.mk:48: Drivers/STM32WBAxx_HAL_Driver/stm32wbaxx_hal_dma_ex.o] Error 1
D:/STM32Cube/I2C_OneBoard_Communication_PollingAndIT_Init/Drivers/STM32WBAxx_HAL_Driver/Src/stm32wbaxx_hal_i2c.c:323:10: fatal error: stm32wbaxx_hal.h: No such file or directory
 323 | #include "stm32wbaxx_hal.h"
 | ^~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [Drivers/STM32WBAxx_HAL_Driver/subdir.mk:50: Drivers/STM32WBAxx_HAL_Driver/stm32wbaxx_hal_i2c.o] Error 1
D:/STM32Cube/I2C_OneBoard_Communication_PollingAndIT_Init/Drivers/STM32WBAxx_HAL_Driver/Src/stm32wbaxx_hal_i2c_ex.c:56:10: fatal error: stm32wbaxx_hal.h: No such file or directory
 56 | #include "stm32wbaxx_hal.h"
 | ^~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [Drivers/STM32WBAxx_HAL_Driver/subdir.mk:52: Drivers/STM32WBAxx_HAL_Driver/stm32wbaxx_hal_i2c_ex.o] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.

 Environment:

CubeIDE 2.0.0, CubeMX 6.16.0, WBA FW 1.8.0, X-CUBE-MEMS1 12.0.0

kclauahBest answer
Associate II
Dec 5, 2025 1:48 AM UTC

Thank you for your suggestion and for pointing me to that guide. I appreciate you taking the time to help.

I followed the steps in the guide you shared, but unfortunately, the project still failed to build.

After some more digging, I eventually found the solution. The issue was that the X-CUBE-MEMS1 pack requires I2C DMA to be enabled, which was not the default configuration in the base project. I found the answer in this forum post: 

https://community.st.com/t5/stm32-mcus/how-to-configure-the-gpdma/ta-p/49412

Once I enabled the appropriate I2C DMA channels in CubeMX and regenerated the code, the build errors were resolved and the project now compiles successfully.

 

2 replies

ST Technical Moderator
Nov 27, 2025 2:03 PM UTC

Hello @kclauah ,

Check if the header files are missing from the generated project structure and ensure that all necessary files are included in the build.

How to integrate the X-CUBE-MEMS1 package with your project

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
kclauahAuthorBest answer
Associate II
Dec 5, 2025 1:48 AM UTC

Thank you for your suggestion and for pointing me to that guide. I appreciate you taking the time to help.

I followed the steps in the guide you shared, but unfortunately, the project still failed to build.

After some more digging, I eventually found the solution. The issue was that the X-CUBE-MEMS1 pack requires I2C DMA to be enabled, which was not the default configuration in the base project. I found the answer in this forum post: 

https://community.st.com/t5/stm32-mcus/how-to-configure-the-gpdma/ta-p/49412

Once I enabled the appropriate I2C DMA channels in CubeMX and regenerated the code, the build errors were resolved and the project now compiles successfully.